Coldfire Linker Command File

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coldfire Linker Command File

1,760 Views
punkinsmasher
Contributor I

Forgive  me. I am extremely new to the Coldfire/CodeWarrior environment. I am using CW 7.2. I have created a very basic project in the CW tool. The readme.txt file tells me that I need to set _FLASHBAR, _IPSBAR, _RAMBAR etc. in the .lcf.

 

Where do I find the .lcf file? One did not show up in the project LCF folder . Yet when I press MAKE, it looks like some basic .lcf must be found somewhere. So......

 

I made a new group (called Linker) and copied a linker command file I found in the tower software for the processor I am using. The build process did not detect that file (or the fact that I wanted to use that file as the .lcf).

 

I have been over every bit of information I can find in the help files, but can not find anything describing how to specify which .lcf file the linker should look at.

 

Any directions are greatly appreciated.

Labels (1)
0 Kudos
Reply
1 Reply

1,167 Views
CrasyCat
Specialist III

Hello

 

Did you create your project using the wizard?

For which Processor?

 

When I create a project with CodeWarrior for Coldfire V7.2, I can see the .lcf file used in the folder Project Settings > Linker Files.

 

The .lcf currently used has a dot in the column with the red target icon on top.

 

Which build target are you trying to build (INTERNAL_FLASH, INTERNAL_RAM, ...)?

 

CrasyCat

0 Kudos
Reply