Coldfire Linker Command File

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Coldfire Linker Command File

1,768 次查看
punkinsmasher
Contributor I

Forgive  me. I am extremely new to the Coldfire/CodeWarrior environment. I am using CW 7.2. I have created a very basic project in the CW tool. The readme.txt file tells me that I need to set _FLASHBAR, _IPSBAR, _RAMBAR etc. in the .lcf.

 

Where do I find the .lcf file? One did not show up in the project LCF folder . Yet when I press MAKE, it looks like some basic .lcf must be found somewhere. So......

 

I made a new group (called Linker) and copied a linker command file I found in the tower software for the processor I am using. The build process did not detect that file (or the fact that I wanted to use that file as the .lcf).

 

I have been over every bit of information I can find in the help files, but can not find anything describing how to specify which .lcf file the linker should look at.

 

Any directions are greatly appreciated.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,175 次查看
CrasyCat
Specialist III

Hello

 

Did you create your project using the wizard?

For which Processor?

 

When I create a project with CodeWarrior for Coldfire V7.2, I can see the .lcf file used in the folder Project Settings > Linker Files.

 

The .lcf currently used has a dot in the column with the red target icon on top.

 

Which build target are you trying to build (INTERNAL_FLASH, INTERNAL_RAM, ...)?

 

CrasyCat

0 项奖励
回复