Coldfire BDM problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coldfire BDM problems

1,987件の閲覧回数
tony_49512
Contributor I

Hi:

 

I am writing some code to program the flash memory of a ColdFire

MCF5270 via the BDM interface.

 

The basic code seems to work. After resetting the device (with

*BKPT asserted) I disable the watchdogs, disable *CS0 and  disable

the cache. The DBM never returns any error during all this and the

values written are read back and verified to be correct.

 

The next step would be to access the internal SRAM. To this end I

program the RAMBAR register with 0x10000001 to place the start

of the SRAM memory (64K) at 0x10000000. Again, the value is read

back from the RAMBAR and verified to be correct.

 

After this, ever access to the SRAM memory fails: Regardless of what 

I write, the interface returns the same value. The value returned

(0x2000FFFC) might not mean anything but is is also quite interesting

because it looks like the reset value of a stack pointer (location 0 in

boot ROM for the Coldfire) that I would load to point to the top of a

64KB memory. It seems to imply that *CS0 is  active and the value

read is from the external flash rather than the internal SRAM, but

having disabled *CS0 this seems strange.

 

Since the BDM never returns any error I am tempted to think that

the basic code works, and that writing to the SRAM is only a matter

of programming some other registers: I am only mildly familiar with

the Coldfire core, so at this point I am looking for ideas.

 

Any help will be appreciated. 

 

Tony 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,157件の閲覧回数
polofermin
Contributor III

Hello, Do you have USB port?

 

Bye!

0 件の賞賛
返信