Codeworrior serdes Protocol/Speed Configuration window is not complete

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codeworrior serdes Protocol/Speed Configuration window is not complete

ソリューションへジャンプ
5,060件の閲覧回数
muaxi8
Contributor V

my custom board is lx2160a,serdes2 protocol is 7.

Click the Change protocol and speed configuration button

muaxi8_3-1634698117939.pngmuaxi8_3-1634698117939.png

The figure below presents an overview of the Protocol/Speed Configuration window。
The protocol content in red box seems incomplete, no SGMII, USXGMII,it is Normal?
muaxi8_4-1634698219591.pngmuaxi8_4-1634698219591.png

 

 

0 件の賞賛
返信
1 解決策
5,055件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download the latest com.freescale.armv8.11.5.5.GA.Win.updatesite.210930.zip release from the following link.

链接: https://pan.baidu.com/s/1pC7eL1SWVruepofVwEedcg

提取码: nt2r 

Then install it in CodeWarrior IDE from Help->Install New Software->Add->Archive.

Please refer to my attached screenshot.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,056件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download the latest com.freescale.armv8.11.5.5.GA.Win.updatesite.210930.zip release from the following link.

链接: https://pan.baidu.com/s/1pC7eL1SWVruepofVwEedcg

提取码: nt2r 

Then install it in CodeWarrior IDE from Help->Install New Software->Add->Archive.

Please refer to my attached screenshot.

0 件の賞賛
返信
5,049件の閲覧回数
muaxi8
Contributor V

after update

muaxi8_0-1634711623934.pngmuaxi8_0-1634711623934.png

 

0 件の賞賛
返信
4,948件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello muaxi8,

Has the problem "Page failed to initialize" been resolved?

 

Thanks,

Yiping

0 件の賞賛
返信
4,944件の閲覧回数
muaxi8
Contributor V

No solution, but I don't need this function anymore。

0 件の賞賛
返信
4,939件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Do you use Chinese edition Window 10 OS? It seems that QCVS serdes tool isn't compatible with Chinese edition Window 10 OS.

0 件の賞賛
返信
5,038件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please create a new project in the new workspace.

0 件の賞賛
返信