Codewarrior and Eclipse.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior and Eclipse.

1,445 Views
infoclog
Contributor III

I downloaded the eclipse version of Code warrior and wanted to know if it will work with my controller MPC5604B. If yes, why do we have a parallel development for CodeWarrior IDE?

Labels (1)
0 Kudos
Reply
1 Reply

1,161 Views
CrasyCat
Specialist III

Hello

 

According to the product page

    http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH

 

CodeWarrior for MCU Eclipse v10.1 supports following Qorivva processors:

 

Qorivva MPC56xx

  • MPC560xP: Qorivva 32-bit MCU for Chassis Applications
  • MPC567xK: Qorivva 32-bit Microcontroller for ADAS Applications
  • MPC564xL: Qorivva 32-bit MCU for Chassis and Safety Applications

 

So MPC5604B does not seem to be supported there.

 

CrasyCat

0 Kudos
Reply