Codewarrior Profiler for MPC565

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior Profiler for MPC565

3,117件の閲覧回数
vijayl
Contributor I
Hi
I have a problem using the codewarrior profiler. I am using running my application from EEprom location 0x0000 with the ROM version selection. After I do the neccesary steps i.e. turn the profiler on, call the init function with proper timebase, terminate it,  and run it on target,  the program crashes. Can someone help me out with this.
 
Thanks,
Vijay
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,478件の閲覧回数
marc_paquette
Contributor V

I apologize for the delay in responding.

Attached is a project that successfully invokes the profiler for an Axiom board. This is the closest reproducible case that our tech support team could come up with given the information you've posted.

Let me know if this helps.

Marc.

0 件の賞賛
返信