Codewarrior MPC55xx V5.90 Command line issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior MPC55xx V5.90 Command line issue

2,252件の閲覧回数
jackzhou
Contributor I
Hello,
 
CodeWarrior MPC55xx,i want to use tcl script,when i
use the command:
cmdIDE /d script.tcl
It prompt:
ERROR:Bad Debug Executable argument (enclose debug-IDE in "quotes").(Code 11)
 
And the script.tcl is:
debug
reset
go
exit
 
Regards,
Jack
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,230件の閲覧回数
Voxan
Contributor III
Hi there,

CW 55xx is special as this tool chain is build only, there is no debugger included in the package.
So any call to the debugger will end like this...

Hope this helps...

Regards
0 件の賞賛
返信