Codewarrier MobileGT V9.2, compiler crash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrier MobileGT V9.2, compiler crash

2,058 次查看
martinw
Contributor III

Hi,

 

Due to wild typing on my part, I had the following include statement in a c module:

 

#include (string.h")

 

 

thats Shift-9 and Shift-0 as the brackets.

 

When compiled, Codewarrier gives an exception and crashes. It seems to be repeatable!

 

I've attached the log file generated by code warrier.

 

MEM_FREE.b2527.20090813.123639A.zip

 

Message Edited by t.dowe on 2009-09-04 02:56 PM
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,349 次查看
CrasyCat
Specialist III

Hello

 

Please submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.

CrasyCat

0 项奖励
回复

1,349 次查看
martinw
Contributor III
ok, I've raised the service request.
0 项奖励
回复