CodeWarrior frustration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior frustration

6,703件の閲覧回数
eswierk
Contributor I
This message is a bit of a rant, but I hope you will forgive the tone and consider it constructive feedback.

I'm an engineer working for a company developing products using Freescale's 32-bit embedded PowerPC processors. My job is to get our Linux-based software running on the evaluation board in preparation for the arrival of our own prototype hardware. I'm using an evaluation board from Embedded Planet and the USB TAP interface from Freescale. As far as I can tell, both are very nicely designed pieces of hardware.

Unfortunately, a major obstacle stands between me and that goal, and its name is CodeWarrior.

The _only_ thing I need CodeWarrior to do is to let me transfer code from my laptop to the flash memory on the board via the USB TAP. One would think the only software necessary for such a task is some sort of file transfer utility. But as the name implies, the CodeWarrior USB TAP can only be controlled from within the CodeWarrior IDE.

-> Why must I install an entire graphical integrated development environment, if all I want to do is transfer a file? I already have a great set of development tools: a text editor, a debugger, a gcc toolchain, a make program, a kernel, a boot loader. I do not want to switch to CodeWarrior, and every minute I'm forced to deal with extraneous tools is a minute (or hour, or day) wasted.

So I hold my nose and open up the CodeWarrior CD package. Now I've got to choose between a CD labeled CodeWarrior Development Studio PowerPC ISA Edition for Comm Processors v8.6 and one labeled CodeWarrior Development Studio for PowerPC ISA Linux Platform/Application Edition v2.6.

-> Put yourself into the shoes of a new user. Do all those extra words give you any clue whatsoever as to the purpose of the CD?

I pop in the first CD, which I'll call CWDSPIEfCP for short. Whoops, I'm running Linux, and all I see are .exe's!

-> If you ship two versions of CodeWarrior, one for Windows and one for Linux, and you aren't bashful about lengthy product names, why not include the word "Windows" somewhere in the name of the Windows version?

So I try the second CD, CWDSfPILP/AE. This one is indeed what I'm looking for. I run the installation program, which grinds away for a while and then informs me it's looking for a Java Virtual Machine.

-> Why in the name of all that is good and right do I need a Java Virtual Machine to copy a bunch of files from the CD to /usr/local/Freescale? Even the Sun Java Virtual Machine itself, certainly not a trivial piece of software, can be installed using rpm!

I wade through the very Windowsy installer, answering mandatory yet irrelevant questions like which gcc toolchain do I want (already got one, thanks!), and finally get around to running CodeWarrior. After a little bit of sleuthing I discover that the program I need to run is /usr/local/Freescale/CodeWarriorIDE/CodeWarrior/CodeWarrior_IDE.

-> The single most important file among the thousands I just installed (not counting the useless toolchain) ought to live in the top-level directory, not buried three levels deep.

-> Typing /usr/local/Freescale/CodeWarriorIDE/CodeWarrior/CodeWarrior_IDE should have the same effect as first cd'ing to /usr/local/Freescale/CodeWarriorIDE/CodeWarrior and then typing ./CodeWarrior_IDE. It should not simply crash complaining about a missing shared library called libxerces-c.so.22.

I run CodeWarrior_IDE, and here the real fun begins: a dialog box pops up (complete with cool retro 1984 Macintosh font) scolding me about a missing license key and telling me to follow the instructions on the registration card. When I click OK, the program dumps a backtrace.

I dig the registration card out of the box (which helpfully suggests registering the product "immediately, or within 15 days" ) and am again stumped: I'm told to "enter the registration code from this registration card" into the form on the web site. Guess what: the space under the words "Your registration number" is blank.

-> What is the point of a registration card that does not include a registration number?

The card also suggests that I email [email protected] if I have any questions about registration or activation (those aren't the same thing?). Well, I really do want to get some work done _now_, not in a day or three, so I try my luck on the web site instead.

I go to freescale.com/cwregister, click Registration and Activation, and enter the Registration and Licensing System. There I'm prompted for a Product or Support Registration Code. (Would that be the same as the registration number that wasn't printed on the card?) I don't have one of those, so I click Need to Register an Evaluation instead.

Now I'm presented with a list of eight Available Evaluations with similar but equally incomprehensible names, none of which matches CWDSfPILP/AE exactly. CodeWarrior for PPC ISA, Linux Application Edition Host sounds close enough, so I click that one, take a brief detour through creating a Freescale username and password, and finally am told to expect an email with an activation code shortly.

When I receive that email, I follow the instructions, which take me on another journey through the Freescale web site, this time copying the authorization code from the email into a web form.

-> If you generate a random 25-character code and email it to me, why do I then have to immediately regurgitate it to you? Couldn't you just remember it for me? Is my time really less valuable than your disk space?

Now I get to choose what kind of Node Lock ID I want: Ethernet Address, Solaris HostID, Dongle ID, or Disk ID. I'm not running Solaris, my disk doesn't have an ID, I don't even want to know what a dongle is, and "None of the Above" is not among the choices, so I choose Ethernet Address. I copy and paste the MAC address from my Ethernet configuration to the field and click Continue. The site promptly barks at me for leaving colons in the address, so I carefully delete each one and try again.

-> Text entry fields for phone numbers, IP addresses, MAC addresses and the like should be intelligent enough to handle spaces, dashes and colons. Come on, this is 2007!

-> If my laptop crashes and I have to switch to another one with a different MAC address, I get to go through this whole process again? I'd better guard my laptop like my first-born.

Finally the web site provides what I need: a license file. Unfortunately the file's contents are embedded right there in the page text; there's no link I can click on to download it. And there's no hint of where I'm actually supposed to put the file. So I copy and paste the contents to /usr/local/Freescale/CodeWarriorIDE/license.dat, and try running CodeWarrior. Nope, still no valid license. But now I notice that farther up in the backtrace is the full path of the license file it's expecting, so I move the file to /usr/local/Freescale/CodeWarriorIDE/CodeWarrior/license.dat, and try once more.

Victory! The IDE starts!

Well, not quite. Now I copy a bunch of board-specific files from another CD from Embedded Planet to the CodeWarrior tree. This itself was an involved process, but I won't get into it here.

I plug in the USB TAP, configure the Flash Programmer settings in CodeWarrior, and try a simple flash operation: computing the checksum of a region of flash memory on the board.

I click Calculate Checksum, the LEDs on the USB TAP start blinking very encouragingly. But then, another dialog box: "Unable to use the plugin 'EPPC Flash Programming'. It is licensed and a valid license key was not found."

You've _got_ to be kidding.

After hours of struggling with registrations and activations and licenses, I'm still not worthy to program the flash on my own board. Time to email [email protected], switch off the computer, and go to bed.

If you've read this far, I congratulate you on your stamina and hope you at least found it entertaining. If you work for Freescale, please take some time to consider this:

-> If a person goes to the trouble of purchasing a Freescale evaluation board, odds are pretty good that he will want to use the CodeWarrior software that the vendor helpfully includes with it. If a person has not purchased a Freescale evaluation board, the chances that a person will want to use CodeWarrior are essentially zero. Therefore, forcing CodeWarrior users to get a PhD in Freescale Licensing solves a problem that does not exist--criminals trading bootleg copies of CodeWarrior--and punishes your actual customers.

-> Please, please, please: stop hurting your customers. We're only trying to use your really cool hardware products, and even help you sell lots more of them. We are not criminals. Our time is valuable, so stop wasting it.

I just hope I can get that flash programmed tomorrow, or next week maybe.
ラベル(1)
タグ(1)
0 件の賞賛
返信
8 返答(返信)

3,281件の閲覧回数
CrasyCat
Specialist III
Hello
 
I can understand your frustration here and I agree with you that this is way too complex.
I want to thank you for the time you spend explaining all the trouble you have gone through.
 
I have forwarded your feedback to the CodeWarrior marketing team and to the people managing the
product.
This should give them valuable information on what need to be improved.
 
So if I understood well you are still looking for a license file enabling flash programming on Linux with CodeWarrior Development Studio for PowerPC ISA Linux Platform/Application Edition v2.6..
Am I right?
 
I will check if I can do something to get you out of here.
 
I am really sorry about all the trouble you have gone through.
 
CrasyCat
0 件の賞賛
返信

3,281件の閲覧回数
eswierk
Contributor I

CrasyCat wrote:


So if I understood well you are still looking for a license file enabling flash programming on Linux with CodeWarrior Development Studio for PowerPC ISA Linux Platform/Application Edition v2.6..

Am I right?




Precisely.

And while you're at it, I would love to know how exactly I can get a license that will last longer than 30 days, both for CodeWarrior and for flash programming.

--Ed
0 件の賞賛
返信

3,281件の閲覧回数
CrasyCat
Specialist III
Hello
 
I will send you a temporary license file for CodeWarrior Embedded Linux V2.6 valid till April 1st through a private message.
 
If you wish to get a longer term license file, you need to purchase it.
You can order on line or through a Freescale distributor.
 
In order to get more details on how you can order a license go to
and click on Buy.
 
Finally, I am not an expert in embedded Linux, but as far as I remember, you only need flash programming to get UBOOT on the hardware board.
After you have burned UBOOT on your board you can program the flash through UBOOT.
UBOOT includes flash programming functionality.
If I remember well, flash is programmed over Ethernet (I am not sure here as I did not do any Linux stuff since a long time).
 
Do you have a working UBOOT for your hardware board? Or is UBOOT available on the board?
 
CrasyCat
0 件の賞賛
返信

3,281件の閲覧回数
eswierk
Contributor I
CrasyCat wrote:


If you wish to get a longer term license file, you need to purchase it.

You can order on line or through a Freescale distributor.


In order to get more details on how you can order a license go to


and click on Buy.





Well, I already tried that, but could not find the Linux version of CodeWarrior until just now I clicked on "CodeWarrior for PowerPC ISA Comm Processors (Windows)". Silly me...




Finally, I am not an expert in embedded Linux, but as far as I remember, you only need flash programming to get UBOOT on the hardware board.

After you have burned UBOOT on your board you can program the flash through UBOOT.

UBOOT includes flash programming functionality.

If I remember well, flash is programmed over Ethernet (I am not sure here as I did not do any Linux stuff since a long time).


Do you have a working UBOOT for your hardware board? Or is UBOOT available on the board?





U-Boot is already installed on my board, but I want to load and test a newer version. I'm not altogether confident in my ability to debug code just by staring at it, so I expect that it won't boot at all on the first try, leaving me with a brick unless I can reprogram the flash some other way.

--Ed
0 件の賞賛
返信

3,281件の閲覧回数
alager
Contributor II
Funny, I found this thread while trying to get my eval board working.  I'm on a windows platform, and I must say, one year later almost none of the issues mentioned above have changed. 

An overly complicated process on every level indeed!




0 件の賞賛
返信

3,281件の閲覧回数
CrasyCat
Specialist III
Hello
 
 I just realize I cannot attach a file to a private message.
 
So find attached a temporary license file valid till April 1st for your CW EPPC Linux Platform edition V2.6. 
 
CrasyCat
0 件の賞賛
返信

3,281件の閲覧回数
Nabla69
Contributor V
Hello,
 
To get a license that last longer than 30 days, the simpler way is to pay for it !
The free full license is for 30 days, anything more is a gift on top.
 
Regards,
A.
0 件の賞賛
返信

3,281件の閲覧回数
peg
Senior Contributor IV
Welcome to Codewarrior,
 
The journey has only just begun...........................
 
0 件の賞賛
返信