CodeWarrior_Connect

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior_Connect

1,515 Views
787316657
Contributor I

Hello,

The development board of the LS1043ARDB we are using is currently connected. When clicking on the 1 and 2 in the figure, the A area will display the connection to the four COREs, but when we click Diagnose Connect, the fourth button is shown, B The region will be consistent in this state, what will be the cause?

Thanks!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,394 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello 晓 刘,

Please attach the figures which you mentioned.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply