CodeWarrior Cache view does not behave as expected (or e5500 issue?)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Cache view does not behave as expected (or e5500 issue?)

ソリューションへジャンプ
2,070件の閲覧回数
mathiasparnaude
Contributor III

Hi,

 

I use CodeWarrior Development Studio 10.4.0 with a T1040RDB board. I am investigating a strange behaviour around L1 caches of the e5500 core (mine is Version: 2.0, 0x80241020) . I wanted to find help with the Cache view in CodeWarrior but that is even more strange...

 

Are there any errata documents about e5500 caches? I haven't found.

 

Anyway, here is the initial purpose of my post:

 

Description

 

U-Boot locks 3 ways of the L1 data cache. When I stop U-Boot with the CodeWarrior debugger (just after the DRAM initalization) to inspect the cache, I see:

 

All locked cache lines have a different address and LRU but other properties are the same:

- Dirty: Yes

- Lock: Yes

- Valid: Yes

- Share: No

- Data: zero values

 

Comments and questions

 

1. The first strange point is the data content. U-Boot locks some ways to use this space as memory. Is the view known to miss some things (like data display)?

 

2. In the cache view context menu, I choose "Flush" but the only property that changes is "Valid", that is set to "No". That should not change this property but "Dirty".

If instead of "Flush", I choose "Invalidate", properties "Dirty" and "Valid" are set to "No", as expected.

 

3. Still from the menu, if I choose "Invalidate Line" or "Flush Line", the result is the same: lines are turned "Dirty: Yes" and "Valid: No". That does not seem to be coherent.

 

4. Setting a breakpoint in the U-Boot code, I execute flush_dcache(), that has no effect, I still see: "Dirty: Yes", "Lock: Yes", "Valid: Yes"... The lines should be cleaned.

Just after, I call invalidate_dcache(), and I get: "Dirty: No", "Lock: Yes", "Valid: No".

 

5. After a printf, I see that some lines are shown are "Lock: No"! How is it possible? Is there a problem with the "Cache" view or in an lower-level part?

 

Thanks,

 

Mathias

ラベル(1)
0 件の賞賛
返信
1 解決策
1,855件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Mathias Parnaudeau,

I use CodeWarrior 10.5 to connect the T1040RDB board, when the cache able data are accessed, they all could be viewed correctly in the content table. So I think the data display depends on if they've been load into cache line.

For the "Flush" operation, it's normal the "Valid" changing to "NO", as I understand, flush means data written back from cache to memory and invalidation corresponding cache. See below:

pastedImage_0.png

In the same way, "Invalidate" and "Flush" looks similar in the cache, the difference is whether data is written back.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,856件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Mathias Parnaudeau,

I use CodeWarrior 10.5 to connect the T1040RDB board, when the cache able data are accessed, they all could be viewed correctly in the content table. So I think the data display depends on if they've been load into cache line.

For the "Flush" operation, it's normal the "Valid" changing to "NO", as I understand, flush means data written back from cache to memory and invalidation corresponding cache. See below:

pastedImage_0.png

In the same way, "Invalidate" and "Flush" looks similar in the cache, the difference is whether data is written back.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,855件の閲覧回数
mathiasparnaude
Contributor III

Thank you, lunminliang.

I missed that: dcbf flushes and invalidates the data cache block. So that turns off the Valid bit. That answers questions 2 and 3 (even if nothing is said about what theoretically happens to the Dirty bit).

And I also see that "dcbst is implemented identically to dcbf".

0 件の賞賛
返信