Code Warrior for PA v10.1.2(evaluation)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Code Warrior for PA v10.1.2(evaluation)

1,355 次查看
gururaj
Contributor I

hi I have installed Code Warrior for PA v10.1.2(evaluation).

 

I a newbie for code warrior. I just wanted to download uboot into the nor flash of my board with p4080 processor.

 

When I checked the flash programmer application of  IDE there was no option for setting the processor type and debugger type(like USB TAP or Ethernet tap)

 

When I browsed the manual I found that have to setup Remote connection system. But I am getting errors  like "not a valid host" and infact i could not set up parent profile name.

 

I am totally confused. Even I do not know what is "Remote Connection System."Please help me or guide me wher I can find the solutions.

Thank You

标签 (1)
0 项奖励
回复
1 回复

1,110 次查看
TomE
Specialist II

You've asked this in the "About the Forums" Forum. You should search the following one, and if that doesn't find anything, post there.

CodeWarrior Development Tools

I pasted the correct link into my post, but then this system CHANGED the link to point to the wrong place.

In order to get around this problem, click on the above link and THEN click on the "Content" tab. I've managed to get around this by editing the raw HTML, so you should be able to click on the following:

http://community.freescale.com/community/codewarrior/content

Tom

0 项奖励
回复