Can't debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't debug

5,227件の閲覧回数
timotay01
Contributor I
When trying to move from the MCF5208EVB to our target board using CF5208 I get the following error when attempting to debug (our board)
"Could not set PC to entry point". This error comes up everytime after it downloads the code to the RAM. I have created a .cfg file to match the differences between the EVB board and ours and using it in a new target profile. Has anyone seen this error before or have some insight into what I could do to try find out what might be wrong on our board?
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,215件の閲覧回数
ElectricMonk
Contributor I
Long time since your post, but I've just had this problem.  It went away once I erased the lowest block of FLASH.  It looks like the processor was running some code (perhaps in user mode) which prevented access to the PC.
0 件の賞賛
返信

2,215件の閲覧回数
armish
NXP Employee
NXP Employee
Hi dear,
 
I am using Coldfire mcf5329 mcu and codewarrior version 5.7. I am also facing the error 'Cant set PC to entry point' 9 out of 10 times, I want to download the code to SRAM of MCU. Could you pls elaborate how did you resolve this problem?
 
Thanks in advance
0 件の賞賛
返信

2,215件の閲覧回数
J2MEJediMaster
Specialist I
OK, just to make sure I got this straight: the program downloads without problems on the eval (EVB) board, but not on your prototype? The error message tends to hint that the debugger isn't getting control of the processor. Are you certain that the debug interface is working properly?

---Tom
0 件の賞賛
返信

2,215件の閲覧回数
timotay01
Contributor I

[TOM] OK, just to make sure I got this straight: the program downloads without problems on the eval (EVB) board, but not on your prototype?

[TIM] Correct

[TOM]The error message tends to hint that the debugger isn't getting control of the processor.

[TIM] Agreed, I will look more closely at the signals from the BDM to the processor.

[TOM] Are you certain that the debug interface is working properly?

[TIM] I assumed it was because it downloads the code fine (Blue downloaad progress bar completes), then the error happens once it tries to start running. Also in my .cfg file I can change the status of an onboard LED (on or off) and it does turn the LED on or off.


---Tom

0 件の賞賛
返信