Can not find vmlinux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not find vmlinux

3,353件の閲覧回数
cengizhanyapici
Contributor I

In my project I want to debug Linux kernel and it's modules by using CodeWarrior 10.5.1 tool with Code Warrior Tap.For this purpose, T1024rdb board is used. Although it has PowerPC architecture,it's stated in the forum that it has the same procedure like ARM arcitecture.So "AN4980.pdf" procedure was taken as a reference.However,when I worked on the document at the part of the "Create ARMV7 project's" fifth step which is"Browse to the vmlinux executable file and Select open." I could not find any executable named as vmlinux. Thank you for your help.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,801件の閲覧回数
addiyi
NXP Employee
NXP Employee

Aftre building the kernel, vmlinux will be placed in a path similar with this one: \build_p4080ds_release\tmp\work\p4080ds-fsl-linux\linux-qoriq\3.12-r0\git\

In CW make sure you change the file type in the lower right corner of the Select file dialog, to all file, because by default is set .elf file.

Adrian 

0 件の賞賛
返信

2,801件の閲覧回数
cengizhanyapici
Contributor I

When I looked into my directory  \poky\build_t1024rdb-64b_release\tmp\work\t1024rdb_64b-fsl-linux\linux-qoriq\3.12-r0\git I still could not vmlinux.You can see the steps below:

[user@localhost poky]$ source ./fsl-setup-poky -m t1024rdb-64b -j 2 -t 2 -l

t1024rdb-64b

Run the following commands to start a build:

bitbake fsl-image-x11

bitbake fsl-image-full

bitbake fsl-image-flash

bitbake fsl-image-virt

bitbake fsl-image-core

bitbake fsl-image-minimal

To return to this build environment later please run:

. /yocto/QorIQ-SDK-V1.8-20150619-yocto/poky/build_t1024rdb-64b_release/SOURCE_THIS

[user@localhost build_t1024rdb-64b_release]$ pwd

/yocto/QorIQ-SDK-V1.8-20150619-yocto/poky/build_t1024rdb-64b_release

[user@localhost build_t1024rdb-64b_release]$ ls

conf SOURCE_THIS

[user@localhost build_t1024rdb-64b_release]$ source SOURCE_THIS

Back to build project /yocto/QorIQ-SDK-V1.8-20150619-yocto/poky/build_t1024rdb-64b_release.

[user@localhost build_t1024rdb-64b_release]$ PWD

bash: PWD: command not found...

Similar command is: 'pwd'

[user@localhost build_t1024rdb-64b_release]$ Pwd

bash: Pwd: command not found...

Similar command is: 'pwd'

[user@localhost build_t1024rdb-64b_release]$ pwd

/yocto/QorIQ-SDK-V1.8-20150619-yocto/poky/build_t1024rdb-64b_release

[user@localhost build_t1024rdb-64b_release]$ bitbake fsl-image-minimal

Parsing recipes: 100% |#####################################################| Time: 00:07:47

Parsing of 1846 .bb files complete (0 cached, 1846 parsed). 4209 targets, 192 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION = "1.22.0"

BUILD_SYS = "x86_64-linux"

NATIVELSBSTRING = "CentOS-7.3.1611"

TARGET_SYS = "powerpc64-fsl-linux"

MACHINE = "t1024rdb-64b"

DISTRO = "fsl-networking"

DISTRO_VERSION = "QorIQ-SDK-V1.8"

TUNE_FEATURES = "m64 fpu-hard e5500"

TARGET_FPU = "hard"

meta

meta-yocto

meta-yocto-bsp = "daisy:18837ea4cdd4fdab608e0a032a11a2dfb6b1ee1a"

meta-fsl-ppc = "daisy:ed8d8f097eb9fb9c4d76cfeb617da5ce72d9b414"

meta-fsl-toolchain = "daisy:a253b3594d8d9e0a4ed869d1fb502c395c4438ac"

meta-fsl-networking = "daisy:6eb28ed659bbadfa470237dfce98bcbf53c18fe1"

meta-virtualization = "daisy:df44ec7a68c8e4b713a458a5b93e903103dea85c"

meta-oe

meta-networking

meta-webserver

meta-ruby

meta-perl

meta-filesystems = "daisy:4a44c4107899363b22c01eb5621b0c86db1c659c"

meta-java = "daisy:65c89b93fa9d4c89e1dfb5b795075cbadb541009"

meta-openstack

meta-openstack-compute-deploy

meta-openstack-controller-deploy

meta-openstack-qemu

meta-openstack-compute-test-config

meta-openstack-controller-test-config

meta-cloud-services = "daisy:c040904422eb3c13f7abb66996bed8d675ada860"

meta-security = "daisy:9f4c3849521465b459845dcc1a7a885bacaae9d9"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

NOTE: Tasks Summary: Attempted 1584 tasks of which 1312 didn't need to be rerun and all succeeded.

[user@localhost build_t1024rdb-64b_release]$ bitbake -c menuconfig virtual/kernel

Loading cache: 100% |############################################################| ETA: 00:00:00

Loaded 4210 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION = "1.22.0"

BUILD_SYS = "x86_64-linux"

NATIVELSBSTRING = "CentOS-7.3.1611"

TARGET_SYS = "powerpc64-fsl-linux"

MACHINE = "t1024rdb-64b"

DISTRO = "fsl-networking"

DISTRO_VERSION = "QorIQ-SDK-V1.8"

TUNE_FEATURES = "m64 fpu-hard e5500"

TARGET_FPU = "hard"

meta

meta-yocto

meta-yocto-bsp = "daisy:18837ea4cdd4fdab608e0a032a11a2dfb6b1ee1a"

meta-fsl-ppc = "daisy:ed8d8f097eb9fb9c4d76cfeb617da5ce72d9b414"

meta-fsl-toolchain = "daisy:a253b3594d8d9e0a4ed869d1fb502c395c4438ac"

meta-fsl-networking = "daisy:6eb28ed659bbadfa470237dfce98bcbf53c18fe1"

meta-virtualization = "daisy:df44ec7a68c8e4b713a458a5b93e903103dea85c"

meta-oe

meta-networking

meta-webserver

meta-ruby

meta-perl

meta-filesystems = "daisy:4a44c4107899363b22c01eb5621b0c86db1c659c"

meta-java = "daisy:65c89b93fa9d4c89e1dfb5b795075cbadb541009"

meta-openstack

meta-openstack-compute-deploy

meta-openstack-controller-deploy

meta-openstack-qemu

meta-openstack-compute-test-config

meta-openstack-controller-test-config

meta-cloud-services = "daisy:c040904422eb3c13f7abb66996bed8d675ada860"

meta-security = "daisy:9f4c3849521465b459845dcc1a7a885bacaae9d9"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

NOTE: Tasks Summary: Attempted 242 tasks of which 237 didn't need to be rerun and all succeeded.

[user@localhost build_t1024rdb-64b_release]$ bitbake -c virtual/kernel

Nothing to do. Use 'bitbake world' to build everything, or run 'bitbake --help' for usage information.

[user@localhost build_t1024rdb-64b_release]$

 

 

 

 

 

[user@localhost git]$ ls

arch Documentation init lib net security

block drivers ipc localversion-rt README sound

COPYING firmware Kbuild MAINTAINERS REPORTING-BUGS tools

CREDITS fs Kconfig Makefile samples usr

crypto include kernel mm scripts virt

[user@localhost git]$ find . -name "vmlinux"

[user@localhost git]$

0 件の賞賛
返信

2,801件の閲覧回数
addiyi
NXP Employee
NXP Employee

Try the followings:

$ bitbake -c cleansstate virtual/kernel
$ bitbake -c patch virtual/kernel
$ bitbake -c compile -f virtual/kernel
$ bitbake virtual/kernel

Adrian

0 件の賞賛
返信