Can I automate flash programming for M52235EVB with CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I automate flash programming for M52235EVB with CodeWarrior

1,859 Views
hdj100r
Contributor I
Hello,
 
I have a M52235EVB and am using CodeWarrior V6.3. Is there any way to automate the downloading program to flash after a successful make? The debugger seems to automate the downloading to RAM, but my program is too large for the RAM, and I need it in flash. It is becoming a real drag having to manually erase and then program the flash using the flash programmer tools.
 
Cheers
David 
Labels (1)
0 Kudos
Reply
1 Reply

821 Views
CrasyCat
Specialist III

Hello

It is not possible to automatically (or transparently) download code into flash when you hit the debug button.

I will forward that to our planning team as a possible improvement for a future release of the product.

CrasyCat

0 Kudos
Reply