CWTAP Network Setup Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CWTAP Network Setup Issue

1,033 Views
aloishahn
Contributor III

Hi,

 

during networks setup of cwtap I got a bad entry into "netparam static_routes", which I can't delete

 

How can I delete the static_routes entry "0." ?

Otherwise, how could I reset the CWTAP probe EPROM to factory defaults?

 

Any hints welcome.

best regards

Alois

 

------------------------------------

 

                  ####

               ##########

            ##########  ....          Freescale Semiconductor Inc.

               ####  ..........       Copyright (c) 2012

                  ..........  ####    All Rights Reserved

                     ....  ##########

                        ##########    Codewarrior TAP Firmware

                    ....   ####       Boot Loader Version 1.0.1

                 ..........             built Mon Aug 26 18:55:20 UTC 2013

              ..........  ####        OS Version 1.0.2

          ####   ....  ##########       built Mon Oct 28 21:40:28 UTC 2013

       ##########   ##########

    ##########  ....   ####           Main Board: CodeWarrior TAP

       ####  ..........               Probe Tip:  Power Architecture JTAG/COP

          ..........

      ####   ....

   ##########                         Note: This product uses open-source

##########                            components.  See "help license"

   ####                               for details.

 

Network configuration is static:CWTAP05

Using static IP address 172.30.131.65:255.255.255.0

core>

core> netparam

ethernet_address        = 00:04:9F:03:54:4D 

bootconfig              = static:CWTAP05

static_ip_address       = 172.30.131.65:255.255.255.0

static_dns_server       = 172.30.131.254

static_hosts            = <none>

static_routes           = destination     gateway         metric

                          --------------- --------------- ------

                          0.                            

core>

core> netparam delete_route 0.

0.: Unknown host

core> netparam

 

netparam

ethernet_address        = 00:04:9F:03:54:4D 

bootconfig              = static:CWTAP05

static_ip_address       = 172.30.131.65:255.255.255.0

static_dns_server       = 172.30.131.254

static_hosts            = <none>

static_routes           = destination     gateway         metric

                          --------------- --------------- ------

                          0.                             

core>

Labels (1)
0 Kudos
Reply
0 Replies