CW7.1-CF: Command-line vs. GUI operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW7.1-CF: Command-line vs. GUI operation

2,571件の閲覧回数
jbezem
Contributor III

Maybe someone can explain a few quirks I noticed when converting a CW7.1 GUI project to a CW7.1 command-line based GNU Make environment using the command line compiler/assembler/linker:

1. In the project, several assembler source files carry an extension *.cw; the GUI accepts those without complaint; using the CL tools I get the warning: 

 

### Command_Line_Tools/mwasmmcf.exe Driver Warning:#   No file mapping matches '..\..\LLD-C\src\boot\startup\vectors.cw' #   (unrecognized file contents or filename extension); treating as source #   text

 How can I prevent this warning?

2. In my medium-sized project (~2000 source files) I use 3 libraries to be linked together with the main application. When I compile-and-link using the CL tools, I get two unresolved linker warnings:

 

### Command_Line_Tools/mwldmcf.exe Linker Error:#   Undefined : "__heap_addr"#   Referenced from "init_default_heap" in C_4i_CF_StdABI_MSL.a### Command_Line_Tools/mwldmcf.exe Linker Error:#   Undefined : "__heap_size"#   Referenced from "init_default_heap" in C_4i_CF_StdABI_MSL.a

 I've seen samples defining these items in the *.LCF file, but my code doesn't contain definitions for them, however, the GUI manages to produce a valid executable, without apparently defining them either. Is there some implicit definition from the GUI-side that I have to handle myself when using the CL?

3. When I perform a clean CL-build, building everything from scratch, I just get the two warnings from issue 2. If I do an incremental build, several but not all files are recompiled (dependency checking currently is limited), libraries are recreated. But curiously, the linker produces an additional set of unresolved references from another two files that aren't a problem for a full build. Yes, I know CW is using a positional linker, but I verified the linker instructions to be identical...

Is the linker implicitly updating a library if it already exists, leaving identical objects alone and appending changed objects again to the end?

 

TIA for any clarification possible.

 

Johan

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,383件の閲覧回数
jbezem
Contributor III

OK, issues 2 and 3 have been resolved. 3 was a subtle makefile error, and 2 an ordering issue because of 3.

 

For the warning on assembling *.cw files I would still be grateful for a solution.

 

And an additional question came up: Is the algorithm by which the positional linker tris to resolve references described somewhere? I just found references that the "link order" is instrumental, but no information as to how this link order shall be established, other than "trial and error". Any documentation to that?

 

Thanks,

 

Johan

0 件の賞賛
返信