CW6.3 printf floating point

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW6.3 printf floating point

7,106件の閲覧回数
tartiz
Contributor I
I'm using CW6.3 with M52233DEMO board.
I try to use floating point.
It is OK for calculates but not for printf (?).
 
The followings source code  ( wheare x=1038.110) :
 
printf(sf,"%5.2f\n\r%6.3f\n\r%7.4f\n\r", x, x, x);
 
produce the following output on the uart debug console :
 
%5.2f
%5.2f
%6.3f
%7.4f
 
Why ?
 
 
 
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
7 返答(返信)

3,156件の閲覧回数
J2MEJediMaster
Specialist I
Your printf statement begins with a variable (?) "sf," rather than the control string that describes the formatting to be used. The control string should be the first argument in printf(), not the second one, as it is in your example.

---Tom
0 件の賞賛
返信

3,156件の閲覧回数
tartiz
Contributor I
I have failed the source line .
I'm using the M52233DEMO board and the CodeWarrior 6.3 Special edition.
 
Now there is the correct code for printf test and the output on the UART console.
.
 
/*
 * File:  main.c
 * Purpose:  sample program
 *
 */

#include <stdio.h>
 
char sf[80];
 int i = 25;
   char c = 'M';
   short int d = 'm';
   static char s[] = "Metrowerks!";
   static char pas[] = "\pMetrowerks again!";
   float f = 3.1415926;
   double x = 3.1415926;
   int count;
   int fi;
   int xi;
   float input_f;
  
int main()
{
int count;
  
    printf("\n\r---------------------------------------\n\r");
    printf("Hello World 2 in C\n\r");
 
 fflush(stdout);
 
  
   printf("\n\r\n\r");
   printf("%s printf() demonstration:\n\r%n", s, &count);
   printf("The last line contained %d characters\n\r",count);
   printf("Pascal string output: %#20s\n\r", pas);
   printf("%-4d 0x%x 0x%06x %-5o\n\r", i, i, i, i);
   printf("%*d\n", 5, i);
   printf("%4c %4u %4.10d\n\r", c, c, c);
   printf("%4c %4hu %3.10hd\n\r", d, d, d);
   printf("$%5.2f\n\r", f);
  
   fi=(int)(f*100000000.);
   xi=(int)(x*100000000.);
   printf("fi  (int)(x*1000000000.)=%d\n\r",fi);
   printf("xi  (int)(x*1000000000.)=%d\n\r",xi);
 printf("input float : ");
 scanf("%f",&input_f);
    printf("\n\r  inputf*1000=%d\n\r",(int)(input_f*1000.));
 fflush(stdout);
 while(1); // Idle
 
 return 0;
}

---------------------------------------
Hello World 2 in C

Metrowerks! printf() demonstration:
The last line contained 37 characters
Pascal string output:    Metrowerks again!
25   0x19 0x000019 31
   25
        M   77 0000000077
   m  109 0000000109
$%5.2f
fi  (int)(x*1000000000.)=314159250
xi  (int)(x*1000000000.)=314159260
input float :
  inputf*1000=0
The red line is wrong : should be 3.14
 
And  the scanf  also  is'nt OK :  should be waiting for input from UART console.
 
0 件の賞賛
返信

3,156件の閲覧回数
J2MEJediMaster
Specialist I
Take a close look at the printf() statement that generates that red line. What's that "$" character doing in there, at the start of the control string?

Sorry, I don't know what could be going wrong with the scanf(). Have you tried any of the code examples that might have a scanf() in it?

---Tom
0 件の賞賛
返信

3,156件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
my guess (I'm not so familiar with CF), you are using a non floating point version of the library.
One of the largest parts of printf is its floating point support, therefore I can imagine (not sure for CF) that there is a library with floating point and one without floating point. Which library do you use?
I think it's important not to get the floating point (size) overhead unless you really use it.

Daniel
0 件の賞賛
返信

3,156件の閲覧回数
tartiz
Contributor I
I'm using the default libraries included in the project when I have selected  M52235EVB stationery and  C.
0 件の賞賛
返信

3,156件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
The printf out of the library used in the statinery project does not support to print floating point numbers.
Change it to another library, see the
Help\PDF\Targeting_ColdFire.pdf
manual for details what the library filenames do mean. This manual also explains that the printf support for the size optimized libs does not support floating points.

For example, for the Console Debug build target, use
C_TRK_4i_CF_MSL.a
instead of the size optimized
C_TRK_4i_CF_SZ_MSL.a
library.

Note that my little demo app got about 3 times bigger when switching to the non size optimized library.

Daniel
0 件の賞賛
返信

3,156件の閲覧回数
tartiz
Contributor I
I verified : OK!  for Console debug.
Tanks very much.
Tiziano
0 件の賞賛
返信