CW11.1 for MPC56X Problem2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW11.1 for MPC56X Problem2

1,200件の閲覧回数
NXP_Leo
Contributor II

When i do compile, it report errors below, but i check the lcf file, i can't find where can result this issue

>linker command file 'acnblhdr.obj' is missing from project.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>linker command file 'oemblhdr.obj' is missing from project.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>linker command file 'acnhdr.obj' is missing from project.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>linker command file 'acnhdr.obj' is missing from project.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with executable address
>of .default_eeprom_data section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with ROM image address
>of .default_eeprom_data section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with executable address
>of .algo_parameter section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with ROM image address
>of .algo_parameter section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with executable address
>of .ivor_branch_table section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with ROM image address
>of .ivor_branch_table section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with executable address
>of .__exception_handlers section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with ROM image address
>of .__exception_handlers section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with executable address
>of .init section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with ROM image address
>of .init section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with executable address
>of .init_vle section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with ROM image address
>of .init_vle section.
C:/Freescale/CW MCU v11.1/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Warning
>Overlap of the ROM image address of .text_vle section with executable address
>of .text_vle section.

pictures below are the lcf file screenshot.lcf.PNG

Capture.PNG

 

0 件の賞賛
返信
0 返答(返信)