CW10, Flash programmer.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10, Flash programmer.

1,848 Views
JeffB
Contributor I

Is anyone getting any use out of CW10?

 

I am using an MCF52259 processor  with the PE Multilink, and running CW10 on an XP machine.

This project was imported to CW10 from CW7.1.2.

 

I am choosing the Flash File to Device from the Flash Programmer Icon.  I chose the elf file to program and here are the results as seen in the console window:

 

 

fl::target -lc "CW10 Debug Bootloader - CW10 Debug Bootloader - PEMICRO_USB"

fl::target -b 0x20000000 0xffff

fl::target -v off -l off -ie on -i "C:/Projects/CW10/USB-DebugBootloader/CW10 Debug Bootloader/../cfg/mcf52259_internal_flash.cfg" -p 52259

 

Error: no such processor "52259"

 

How can it not find the processor?

the *.cfg file that it is using is from the debugger section from the original project.

 

Anyone have any ideas of what i need to do?

Labels (1)
0 Kudos
Reply
1 Reply

1,121 Views
GJT
Contributor I

I had the exact same problem and lowered the BDM connection speed to get things working.

 

  1. Click on the “Run” menu item and select “Debug Configurations…”
  2. Click on the “Debugger” Tab and then the “Connection” Tab
  3. In the “BDM Communications Speed” area select a slower BDM_SPEED value (i.e. lower BDM CLOCK FREQ).
0 Kudos
Reply