CW10.5 & FLASH Programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.5 & FLASH Programmer

1,858 Views
lwgong
Contributor I

Hello,

 

We have installed CW10.6.4 and setup the FLASH Programmer as a Task. But the flash programmer actions is not activated. like that:

QQ图片20170721225608.png

How can I do that!!!

Thanks,

Lw

0 Kudos
Reply
2 Replies

1,676 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Lw,

Please install CodeWarrior for PA 10.5.x for QorIQ processors.

There is compatible problem between Chinese edition OS and CodeWarrior, please try the following workaround.

1. I suggest you reinstall CodeWarrior 10.5 in an English edition Window PC if possible.

2. Please change theme of OS, please refer to "4.3.1. Usage Notes and Limitations(Ubuntu Themes)" section in the release note CW_PA_v10.5.x\PA\Release_Notes_PowerArchitecture.pdf.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,676 Views
lwgong
Contributor I

hello, YipingWang, thank you for answer my question.

my host pc os is win7 x64 Chinese edtion

-Original-

0 Kudos
Reply