CW10.5 & FLASH Programmer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW10.5 & FLASH Programmer

1,311 次查看
lwgong
Contributor I

Hello,

 

We have installed CW10.6.4 and setup the FLASH Programmer as a Task. But the flash programmer actions is not activated. like that:

QQ图片20170721225608.png

How can I do that!!!

Thanks,

Lw

标记 (2)
0 项奖励
回复
2 回复数

1,129 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Lw,

Please install CodeWarrior for PA 10.5.x for QorIQ processors.

There is compatible problem between Chinese edition OS and CodeWarrior, please try the following workaround.

1. I suggest you reinstall CodeWarrior 10.5 in an English edition Window PC if possible.

2. Please change theme of OS, please refer to "4.3.1. Usage Notes and Limitations(Ubuntu Themes)" section in the release note CW_PA_v10.5.x\PA\Release_Notes_PowerArchitecture.pdf.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,129 次查看
lwgong
Contributor I

hello, YipingWang, thank you for answer my question.

my host pc os is win7 x64 Chinese edtion

-Original-

0 项奖励
回复