CW debug configuration/ccs issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW debug configuration/ccs issue

2,248件の閲覧回数
SimG
Contributor I

Hello,

I am trying to debug and download hello_world to an embedded p4080. I am using CW v10.0.2 with a USBTAP. I have followed the documentation and set everything up correctly. When I run debug through debug configurations I get the following error:

An Internak error occured during: "Launching hello_world-core0_Hardware_Debug_core0_P4080DS_Download".

 

Details: The function getServiceByContractID returned an error condition (0x80040154)

 

I have checked my USBTAP connection throught ccs by using the command: source IDcode.tcl

I cannot get rid of this function no matter what I try.

 

This is running on Linux, fedora 14. 

Any help is much appreciated. Thank you.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,835件の閲覧回数
SimG
Contributor I

Any clues anyone?!? 

Btw I tired it with windows and it works perfectly fine, so my guess is that I am missing some package for Linux/Fedora and hence the error. 

 

Is there a error log file for code warrior itself so I can go find the file which is giving the error.

Sorry I am new to code warrior!!

 

 

0 件の賞賛
返信

1,835件の閲覧回数
Neih
Contributor I

Hi

 

just to let you know that I got it works fine with Windows as well !

 

Regars

/Neih

 

0 件の賞賛
返信

1,835件の閲覧回数
SimG
Contributor I

So after opening up a service request, I have learned that CodeWarrior is not compatible with Fedora 14 which is bad. Any work arounds possible for this?

0 件の賞賛
返信