CW V6.2 Coldfire, Assembler only

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW V6.2 Coldfire, Assembler only

ソリューションへジャンプ
3,189件の閲覧回数
Bloodhound
Contributor I

Hi All,

 

I'm using the evaluation version of CW V6.2 on a MCF51JM32.

Is there any way to force a new project to only be in assembler? It seems fixed on producing C.

I found an old thread that talked about this with no real answer to the problem.

 

I had been using an older version of CW on a HC08 and that was happy enough to allow the entire project to be assembler from the start.

 

Thanks,

Ross

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,840件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Bloodhound,

 

Assembler only project template is not available in Project Wizard for ColdFire target.

Anyway, you can create such project from scratch and save it into Stationery directory in CodeWarrior install directory (create it if doesn't exist). Then you can use such project as a template when a new project is being created (File -> "New Project..." -> Select your custom stationery).

 

I'd also suggest you to see this thread.

 

Stanish

Message Edited by stanish on 2009-05-13 02:25 PM

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,841件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Bloodhound,

 

Assembler only project template is not available in Project Wizard for ColdFire target.

Anyway, you can create such project from scratch and save it into Stationery directory in CodeWarrior install directory (create it if doesn't exist). Then you can use such project as a template when a new project is being created (File -> "New Project..." -> Select your custom stationery).

 

I'd also suggest you to see this thread.

 

Stanish

Message Edited by stanish on 2009-05-13 02:25 PM
0 件の賞賛
返信
1,840件の閲覧回数
Bloodhound
Contributor I

I should have also had a look through the CW directories, I found -

"\ColdFire V1\Assembly Examples\MCF51QE Demos\MCF51QE32 Demo"

An assembly project all set to go.

 

Thanks,

Ross

 

0 件の賞賛
返信