Target connection device: LS1088A_RDB; Linux OS: ubuntu 20.04.4; CodeWarrior: CW4NET_v2020.06. Tried to connect the target board to debug a demo project thru the CWTAP, and followed the below instruction:
https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Issue-in-code-warrior-for-connecting-to-target-us...
%config cc cwtap:
maximum number of Command Converters reached
config fail
%show cc
0: USB open failure
there are no command converters configured
CWTAP LED status: TX/RX is flashing green, RUN/PAUSE orange.
Let me know any advice or any further information needed. Thanks.