CW 10.0 beta 3 doesn't use __initialize_hardware() that's in cpu.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.0 beta 3 doesn't use __initialize_hardware() that's in cpu.c

Jump to solution
2,775 Views
wdfarmer1
Contributor III

System: CW 10.0 beta 3

Target: MCF51QE128

Language: C++

 

I'm letting Processor Expert do much of the work, and it's constructed an __initialize_hardware() routine in its cpu.c that does what I want, such as turning off the watchdog and enabling the external reset input.  However, that code isn't getting included in my build.  Instead, it was using a different (empty) __initialize_hardware() function that was declared with "#pragma overload" in startcf.c , even though "#pragma overload" is supposed to make that a weak symbol that would be replaced by my function.

 

I've commented out the startup.c function, but now a new __initialize_hardware() function has taken precedence; that code just clears D0-D7 and A0-A4 and then returns.  Perhaps that code came from the EWL library.

 

What can I do to have the linker use the __initialize_hardware() function that's in cpu.c?  I see no way to specify link order in CW 10.0 beta 3.

 

Wayne

Labels (1)
0 Kudos
Reply
1 Solution
1,542 Views
CompilerGuru
NXP Employee
NXP Employee

Did you create a C++ project?

 

I did not see this bug when creating a C project, but for a C++ project the wizard enables "Force C++ Compilation" in the settings

(which I find a bit unfortunate if you ever want to mix real C code with C++ code). This option causes that the processor expert module gets compiled as C++, hence the __initialize_hardware gets name mangled.

View solution in original post

0 Kudos
Reply
4 Replies
1,542 Views
wdfarmer1
Contributor III

Follow-up:  Yes, the 2nd substitute __initialize_hardware() function did come from the EWL library:  the EWL runtime Coldfire library's librt.a which had been built from CF_startup.c long ago.  CF_startup.c's function is marked with the "#pragma overload" just like the startcf.c's is:

 

/* *    Dummy routine for initializing hardware.  For user's custom systems, you *    can create your own routine of the same name that will perform HW *    initialization.  The linker will do the right thing to ignore this *    definition and use the version in your file. */#pragma overload void __initialize_hardware(void);asm __declspec(register_abi) void __initialize_hardware(void){    clr.l    d0    clr.l    d1    clr.l    d2    clr.l    d3    clr.l    d4    clr.l    d5    clr.l    d6    clr.l    d7    movea.l    #0,a0    movea.l    #0,a1    movea.l    #0,a2    movea.l    #0,a3    movea.l    #0,a4 rts}

 

So I still have my problem.  How can I get startcf.c's call to __initialize_hardware() to invoke the __initialize_hardware() routine in the Processor Expert's cpu.c, rather than this runtime version?  cpu.c is located in my "(project name)/Generated Code" subdirectory.

 

Wayne

0 Kudos
Reply
1,542 Views
wdfarmer1
Contributor III

Follow-up:  perhaps part of the problem is mixed assembly code and C/C++ code:

 

The startcf.c caller invokes __initialize_hardware() from ColdFire V1 assembly code:

 

asm __declspec(register_abi) void _startup(void){ /* disable interrupts */    move.w        #0x2700,sr /* Pre-init SP, in case memory for stack is not valid it should be setup using    MEMORY_INIT before __initialize_hardware is called */ lea __SP_AFTER_RESET,a7;    /* initialize memory */    MEMORY_INIT /* initialize any hardware specific issues */    jsr           __initialize_hardware /* setup the stack pointer */    lea           _SP_INIT,a7    /*    (etc.)    */    rts

and that's the call that is getting matched with the __initialize_hardware() function from the EWL library, as noted above.  That library function is also written in ColdFire v1 assembly language.

 

However, the cpu.c source file created by Processor Expert defines __initialize_hardware in C (or C++, if C++ compilation is forced by a compile flag):

 

/*** ===================================================================**     Method      :  __initialize_hardware (component MCF51QE128_64)****     Description :**         Configure the basic system functions (timing, etc.).**         This method is internal. It is used by Processor Expert only.** ===================================================================*/void __initialize_hardware(void){  /* ### MCF51QE128_64 "Cpu" init code ... */  /*  PE initialization code after reset */  /* Common initialization of the write once registers */  /* SOPT1: COPE=1,COPT=1,STOPE=0,WAITE=1,??=0,RSTOPE=0,BKGDPE=1,RSTPE=1 */  setReg8(SOPT1, 0xD3);                 /*(etc.)*/}

Can someone clear up this issue of symbol resolution for me?

 

I don't want to modify the cpu.c routine, since that's regenerated by Processor Expert whenever there's a change in the CPU properties, so the change would have to be made in the startcf.c routine instead.  Do I need a wrapper function to go from assembly to C/C++?

 

Wayne

0 Kudos
Reply
1,543 Views
CompilerGuru
NXP Employee
NXP Employee

Did you create a C++ project?

 

I did not see this bug when creating a C project, but for a C++ project the wizard enables "Force C++ Compilation" in the settings

(which I find a bit unfortunate if you ever want to mix real C code with C++ code). This option causes that the processor expert module gets compiled as C++, hence the __initialize_hardware gets name mangled.

0 Kudos
Reply
1,542 Views
wdfarmer1
Contributor III

Good catch!  That was exactly the problem.  I had created the project as a C++ project, and "Force C++ Compilation" was checked on in Project Properties / ColdFire Compiler / Language Settings.  Unchecking that caused the __initialize_hardware code in cpu.c to be included.

 

I had also included Processor Expert component Term (which included inherent component AsynchoSerial), and the Watchdog component .  Those are defined in .c and .h sources, but my code that calls them is a .cpp and .hpp source, and so generated C++ external names from their prototypes.  That caused their entry points to be undefined symbols during the link.  (I had kept the Force C++ Compilation option to cure that problem.)  I fixed the problem instead by changing my calling code's C++ mode to C for the includes of the component .h sources:

 

#pragma cplusplus off#include "Term1.h"              // asynchronous serial terminal#include "Inhr1.h"              // asynchronous serial device#include "WDog1.h"              // watchdog timer#pragma cplusplus reset

 Thanks!  You get credit for the solution.

 

Wayne

0 Kudos
Reply