CPRI VSS buffer size cause an error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPRI VSS buffer size cause an error

Jump to solution
2,236 Views
xinshuozhang
Contributor I

Hello

I am using B4860SOC. When I set the CPRI VSS buffer size big, the test demo will have a MMUInit error.

How can I find the problem?

Labels (1)
0 Kudos
Reply
1 Solution
2,059 Views
lunminliang
NXP Employee
NXP Employee

Hello xinshuo zhang,

Can you please be more specific?

What buffer do you modify? From what size and to what size?

Is the error during building or running? Can you provide more information?

Thanks.

Regards

Lunmin

View solution in original post

0 Kudos
Reply
2 Replies
2,060 Views
lunminliang
NXP Employee
NXP Employee

Hello xinshuo zhang,

Can you please be more specific?

What buffer do you modify? From what size and to what size?

Is the error during building or running? Can you provide more information?

Thanks.

Regards

Lunmin

0 Kudos
Reply
2,059 Views
xinshuozhang
Contributor I

你好,

我使用的是CW10.8.3

每一路CPRI的速率设置成2.457G,以太网的P指针设置成20

这个时候每个cpri模块的vss_tx_buffer 4行4列4字节,程序运行正常

修改每一路CPRI的速率设置成2.457G,以太网的P指针设置成62

这个时候每个cpri模块的vss_tx_buffer 46行4列4字节,程序在初始化的时候出错,MMUinit错误

还有我们现在想把PA侧的DDR修改成4G,这个时候怎么修改DSP的l3k文件呢?

0 Kudos
Reply