CPRI VSS buffer size cause an error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPRI VSS buffer size cause an error

ソリューションへジャンプ
2,294件の閲覧回数
xinshuozhang
Contributor I

Hello

I am using B4860SOC. When I set the CPRI VSS buffer size big, the test demo will have a MMUInit error.

How can I find the problem?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,117件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello xinshuo zhang,

Can you please be more specific?

What buffer do you modify? From what size and to what size?

Is the error during building or running? Can you provide more information?

Thanks.

Regards

Lunmin

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,118件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello xinshuo zhang,

Can you please be more specific?

What buffer do you modify? From what size and to what size?

Is the error during building or running? Can you provide more information?

Thanks.

Regards

Lunmin

0 件の賞賛
返信
2,117件の閲覧回数
xinshuozhang
Contributor I

你好,

我使用的是CW10.8.3

每一路CPRI的速率设置成2.457G,以太网的P指针设置成20

这个时候每个cpri模块的vss_tx_buffer 4行4列4字节,程序运行正常

修改每一路CPRI的速率设置成2.457G,以太网的P指针设置成62

这个时候每个cpri模块的vss_tx_buffer 46行4列4字节,程序在初始化的时候出错,MMUinit错误

还有我们现在想把PA侧的DDR修改成4G,这个时候怎么修改DSP的l3k文件呢?

0 件の賞賛
返信