CF Flasher Troubles

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CF Flasher Troubles

3,358 次查看
Gian
Contributor I
hi all!
i tried to put colilo in boot-flash (and so erasing DBUG) to avoid the kernel image's download and the net-parameters settings every time. The colilo image has worked from RAM, but NOT from FLASH!!!!!
So now i must restore the DBUG monitor through BDM interface and use CF Flasher... But the CF Flasher seems not work. when i tried to erase the boot flash (i have M5484LITE) it said "could not initialize BDM device".

Do you know why?

My OS is Win2000Professional, the parallel port is setted on "normal" from BIOS, the BDM device is corrected connected (with the 1 pin alligned), and i tried all the jumper's position on the device.
I also installed the P&E Device Drivers, but without results...

Could anyone help me?

Thanks,
Gianluca Salvador
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,733 次查看
Gian
Contributor I
Hi!
searching deeply in the forums i solved my problem thanks to fred_84 and his .dll file, posted here:
http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=159&query.id=11970#M1...
Regards,
Gianluca Salvador
0 项奖励
回复