Debugger can't find MSL source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger can't find MSL source

3,260 Views
nspon
Contributor II
CW for ColdFire, v6.2. Is the debugger meant to be able to step into the MSL source? It switches to assembly every time I do so, it doesn't seem to be able to find the source. I have "Store Full Path Names" turned on, and the debugger finds the source of a library I have built just fine. I can't see what is different about MSL. I can successfully build the MSL library that I am using, and I have tried turning on "A6 stack frames", but to no avail...

I'm actually trying to understand alloc.c so I can figure out how to write free-memory and largest-block routines that scan the heap - if this has already been done somewhere I would love to know...

Thanks for any assistance,
Nigel
Labels (1)
0 Kudos
Reply
2 Replies

2,003 Views
CrasyCat
Specialist III

Hello

MSL library delivered with CodeWarrior for ColdFire 6.2 are generated without debug information. That is the reason you cannot see source code when you are stepping inside of a library function.

If you wish to be able to debug within the MSL library follows these steps:
  - Check which library files you are linking with your application (For Example 
    C_TRK_4i_CF_MSL.a)
  - Open the file {Install}\E68K_Support\msl\MSL_C\MSL_E68k\Project\MSL_C.CF.mcp
   - Activate the build target for the library you are using (for C_TRK_4i_CF_MSL.a
     it is TRK 4i ColdFire)
   - Click next to each if the folder in the column headed with the small green bug. When there is a dot there next to a source file, the compiler will generate debug info for the source file.
   - Rebuild the library.
   - Rebuild the application
You should be able to debug within alloc.c now.

CrasyCat

0 Kudos
Reply

2,003 Views
nspon
Contributor II
Aaargh! Thanks, I missed that one entirely. Thats much better.
0 Kudos
Reply