CCSProtocolPlugin : Error writing memory  [CCS last error: Scan timeout ]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CCSProtocolPlugin : Error writing memory  [CCS last error: Scan timeout ]

20,045件の閲覧回数
kristinkrueger
Contributor II

Hello,

 

I followed the steps in this thread (CW won't debug T4240QDS: fails to reset target), downgraded the FPGA version and now CW gives me the above mentioned new error message. I already updated the drivers and firmware for the CW Tap. I'm working on the T4240QDS under Win7 and I try to run the example baremetal project.

 

Any help will be highly appreciated!

 

Kind regards,

Kristin

ラベル(1)
0 件の賞賛
返信
22 返答(返信)

556件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please try a lower JTAG clock speed (now you have 4000 kHZ). If this not help, try to verify the switch settings to be according with the T4240QDS_eabi_README.txt.

Adrian

0 件の賞賛
返信

557件の閲覧回数
kristinkrueger
Contributor II

I verified the switch settings, they are according to the T4240QDS_eabi_README.txt. Setting the JTAG clock speed to 500/1000/2000 kHz did not solve the problem.

0 件の賞賛
返信