CCS failed to connect after Ubuntu update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCS failed to connect after Ubuntu update

Jump to solution
8,809 Views
vsiles
Senior Contributor I

Hi,

this morning, following an Ubuntu update, I can't manage to connect to my LS1021atwr board anymore.

Here is ccs log:

 

No clients denied (bin) 49 % config cc cmsisdap Identified CMSIS-DAP SERNUM: 20000203C5231E0638DFC1FE Firmware version: 0203 0: CMSIS-DAP (cmsisdap) CC software ver. {0.3} (bin) 50 % ccs::config_server 0 10000 rddi_CMSIS_DAP_DetectNumberOfDevices failed : 0x100d (bin) 51 % 

 

On a second atempt, I get

rddi_CMSIS_DAP_Connect failed : 0x100b

 

I checked th udev rule for cmsis_dap and they are still here.

What could be the cause of these errors ? Any idea on a posible fix ?

 

Best,

Vincent

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
8,221 Views
addiyi
NXP Employee
NXP Employee

Switches looks fine. Try to use directly ccs::config_chain {ls1020a cmsisdap} after config cc cmsisdap.

Adrian

View solution in original post

0 Kudos
Reply
25 Replies
7,519 Views
vsiles
Senior Contributor I

Then I'm sorry but I don't have this image anymore. Thank you for all the support !

0 Kudos
Reply
7,519 Views
addiyi
NXP Employee
NXP Employee

I want the exact image you use. Because, it is possible to have an issue in ccs, but I'm not able to reproduce :smileyhappy:.

Adrian

0 Kudos
Reply
7,518 Views
addiyi
NXP Employee
NXP Employee

Not able to reproduce this issue. Could send me the RCW/Uboot binary?

Adrian

0 Kudos
Reply
7,518 Views
vsiles
Senior Contributor I

I'm sorry but I can't, I don't have any backup of this binary. The one I am using right now is working, with the exact same RCW. Do you want this newer version ?

0 Kudos
Reply
7,521 Views
addiyi
NXP Employee
NXP Employee

Even with all cores in boot hold-off in RCW, the connection must work. Below is the test done on my twr board.

(bin) 52 % config cc cmsisdap

Identified CMSIS-DAP SERNUM: 20000203C5091E5938F5C1A1

Firmware version: 0203

0: CMSIS-DAP (cmsisdap) CC software ver. {0.3}

(bin) 53 % ccs::config_chain {ls1020a cmsisdap}

(bin) 54 % ::ccs::all_run_mode

CortexA7: Reset Mode

CortexA7: Reset Mode

Could you add your RCW?

Adrian

0 Kudos
Reply
7,519 Views
vsiles
Senior Contributor I

Sure,

here is my RCW:

#PBL preamble and RCW header

aa55aa55 01ee0100

#enable IFC, disable QSPI and DSPI

0608000a 00000000 00000000 00000000

30000000 00007900 60640a00 21046000     # cpu0 on hold + secure boot enabled

00000000 00000000 00000000 20000000

00080000 881b7340 00000000 00000000

and if that's relevant, I am using an unmodified board/freescale/ls1021atwr/ls102xa_pbi.cfg

0 Kudos
Reply
7,521 Views
vsiles
Senior Contributor I

my current setting was booting the board with BOOT_HO blocking cpu0. In order to check if the board was damaged, I rebooted from the SD card with a "normal" boot, and it went fine. And now, I can use ccs again.

Maybe some internal state was corrupted and rebooting the board with a "normal" system fixed it ?

Thank you very much for your advices and your time

0 Kudos
Reply
8,222 Views
addiyi
NXP Employee
NXP Employee

Switches looks fine. Try to use directly ccs::config_chain {ls1020a cmsisdap} after config cc cmsisdap.

Adrian

0 Kudos
Reply
7,521 Views
vsiles
Senior Contributor I

In case it helps:

I tried the procedure with SW2.8 set to 1: ccs::config_server 0 1000 answer 'no devices found'

with SW2.8 set to 0: ccs::config_server 0 10000 answer 'rddi_CMSIS_DAP_Connect failed : 0x100b'

The only cable plugged in (except power) is the usb / serial cable

SW2 status: 0 0 1 0 1 1 1 0

SW3 status: 0 1 1 0 0 0 0 1

I boot from SD card using the uboot sd/ifc target of uboot

0 Kudos
Reply
7,521 Views
addiyi
NXP Employee
NXP Employee

You could do the followings checks:

$ ls -lrt /dev/usb

total 0

crw------- 1 root root 180, 96 Jun 17 11:15 hiddev0

$ ls -lrt /dev/hidraw0

crw------- 1 root root 251, 0 Jun 17 11:15 /dev/hidraw0

$ dmesg

....

[3040048.991228] generic-usb 0003:0D28:0204.000B: hiddev0,hidraw0: USB HID v1.00 Device [MBED MBED CMSIS-DAP] on usb-0000:00:1d.0-2/input3

Change udev rules if CMSIS-DAP is recognized only when running CCS as root(sudo) and not as user:

$ sudo emacs /etc/udev/rules.d/mbed.rules

$ SUBSYSTEM=="usb", ATTR{idVendor}=="0d28", ATTR{idProduct}=="0204", MODE:="666"

$ sudo udevadm trigger

Also make sure that "vendor id" and "product id" should match between output from dmesg and udev rules.

For Example:

$dmesg | grep CMSIS

generic-usb 0003:0D28:0204.0001: hiddev96,hidraw0: USB HID ----------------

$ more /etc/udev/rules.d/mbed.rules

SUBSYSTEM=="usb", ATTR{idVendor}=="0d28", ATTR{idProduct}=="0204", MODE:="666"

Adrian

0 Kudos
Reply
7,521 Views
vsiles
Senior Contributor I

No such luck: everything is configured as you explained, and I still get the rddi_CMSIS_DAP_Connect failed: 0x100b

0 Kudos
Reply
7,521 Views
addiyi
NXP Employee
NXP Employee

"rddi_CMSIS_DAP_Connect failed: 0x100b" means: Connection to target failed. Please make sure jtag is not used and SW2.8 is 0.

Adrian

0 Kudos
Reply
7,521 Views
vsiles
Senior Contributor I

I didn't touch the switch for a long time, but to be sure I unplugged the cable, move the switch to 1 and then to 0 again, and replug the cable. Same behavior.

Googling the error messages leads to quite a few post about printer failing to work because of some usb issues, but the fix seems always to patch cups, and I didn't had a cups update this morning, only libc and samba. Maybe something is interfering with the usb driver ?

0 Kudos
Reply
7,521 Views
vsiles
Senior Contributor I

If had a look at dmesg while inserting the USB plug and here is what I get:

May 26 14:38:38 vsiles-Desktop kernel: [17238.769272] usb 1-3.1: new full-speed USB device number 9 using xhci_hcd

May 26 14:38:38 vsiles-Desktop kernel: [17238.860433] usb 1-3.1: New USB device found, idVendor=0d28, idProduct=0204

May 26 14:38:38 vsiles-Desktop kernel: [17238.860436] usb 1-3.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3

May 26 14:38:38 vsiles-Desktop kernel: [17238.860437] usb 1-3.1: Product: MBED CMSIS-DAP

May 26 14:38:38 vsiles-Desktop kernel: [17238.860438] usb 1-3.1: Manufacturer: MBED

May 26 14:38:38 vsiles-Desktop kernel: [17238.860439] usb 1-3.1: SerialNumber: 20000203C5231E0638DFC1FE

May 26 14:38:38 vsiles-Desktop kernel: [17238.861178] usb-storage 1-3.1:1.0: USB Mass Storage device detected

May 26 14:38:38 vsiles-Desktop kernel: [17238.861263] scsi host11: usb-storage 1-3.1:1.0

May 26 14:38:38 vsiles-Desktop kernel: [17238.861716] cdc_acm 1-3.1:1.1: ttyACM0: USB ACM device

May 26 14:38:38 vsiles-Desktop kernel: [17238.864976] hid-generic 0003:0D28:0204.0008: hiddev0,hidraw0: USB HID v1.00 Device [MBED MBED CMSIS-DAP] on usb-0000:00:14.0-3.1/input3

May 26 14:38:38 vsiles-Desktop mtp-probe: checking bus 1, device 9: "/sys/devices/pci0000:00/0000:00:14.0/usb1/1-3/1-3.1"

May 26 14:38:38 vsiles-Desktop mtp-probe: bus: 1, device: 9 was not an MTP device

May 26 14:38:39 vsiles-Desktop kernel: [17239.862574] scsi 11:0:0:0: Direct-Access    MBED    microcontroller  1.0  PQ: 0 ANSI: 2

May 26 14:38:39 vsiles-Desktop kernel: [17239.862989] sd 11:0:0:0: Attached scsi generic sg3 type 0

May 26 14:38:39 vsiles-Desktop kernel: [17239.863353] sd 11:0:0:0: [sdc] 304 512-byte logical blocks: (155 kB/152 KiB)

May 26 14:38:39 vsiles-Desktop kernel: [17239.863544] sd 11:0:0:0: [sdc] Write Protect is off

May 26 14:38:39 vsiles-Desktop kernel: [17239.863548] sd 11:0:0:0: [sdc] Mode Sense: 03 00 00 00

May 26 14:38:39 vsiles-Desktop kernel: [17239.863757] sd 11:0:0:0: [sdc] No Caching mode page found

May 26 14:38:39 vsiles-Desktop kernel: [17239.863760] sd 11:0:0:0: [sdc] Assuming drive cache: write through

May 26 14:38:39 vsiles-Desktop kernel: [17239.874375]  sdc:

May 26 14:38:39 vsiles-Desktop kernel: [17239.875473] sd 11:0:0:0: [sdc] Attached SCSI removable disk

May 26 14:38:39 vsiles-Desktop udisksd[2952]: Mounted /dev/sdc at /media/vsiles/MBED on behalf of uid 1000

As soon as I enter a command is ccs, I get:

May 26 14:38:51 vsiles-Desktop kernel: [17251.899754] usb 1-3.1: usbfs: interface 0 claimed by usb-storage while 'ccs' sets config #1

May 26 14:38:51 vsiles-Desktop kernel: [17251.903352] usb 1-3.1: usbfs: interface 0 claimed by usb-storage while 'ccs' sets config #1

This might be the issue ?

0 Kudos
Reply
7,521 Views
addiyi
NXP Employee
NXP Employee

I get the same messages in dmseg. rddi_CMSIS_DAP_Connect failed: 0x100b, I get only when sw2.8 = 1.

Maybe indeed is something interfering with the usb driver. Did you try a system reboot?

Adrian

0 Kudos
Reply
7,521 Views
vsiles
Senior Contributor I

I just tried to reboot without success. After checking my log for the past few days, I already got some of the "claimed" error messages a couple days ago and everything was fine.

However I got an update from usb 1.3-1 to 1.3-2 which might explain the issue ?

0 Kudos
Reply
7,521 Views
addiyi
NXP Employee
NXP Employee

I'm not sure this could be the reason, because "config cc cmsisdap" works and return the serial number and firmware version from the device.

Do you have other board with cmsis-dap to try on it?

Adrian

0 Kudos
Reply
7,521 Views
vsiles
Senior Contributor I

Unfortunately no, I don't have another board.

This morning I saw that I got new updates from the same package as yesterday. I just tried again after a reboot and nothing changed :/

Vincent

0 Kudos
Reply
7,521 Views
vsiles
Senior Contributor I

Dear addiyi​, I just tried to unplug everything, plug everything back and made a new attempt.

Now the ccs::config_server 0 10000 succeed, but the ccs::config_chain {ls1021a cmsisdap} fails with

LS1020A: Reported SoC topology is inconsistent with real topology.

Maybe this will help to understand what's going on. In the meantime, I'll try to find a new usb cable, maybe the issue is there.

0 Kudos
Reply
7,521 Views
addiyi
NXP Employee
NXP Employee

The correct config chain is: ccs::config_chain {ls1020a cmsisdap}

Adrian

0 Kudos
Reply