Boot and application creation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot and application creation

2,854 Views
Vishwa
Contributor II
I am using Codewarrior IDE with C compiler and developing code for MPC5200 processor. I have to write separate application for Boot and application program. The Boot program has to check whether there is a application in Flash by verifying checksum, if it is there, copy the appication to SDRAM and transfer control to application.
How do I write the boot program and after copying to SDRAM transfer control. Do any one have a sample program and link file to do the same.
Labels (1)
0 Kudos
Reply
2 Replies

1,537 Views
Nouchi
Senior Contributor II
Hello,

You can have a look to U-boot which is a booltloader for several architectures

http://sourceforge.net/projects/u-boot


Emmanuel
0 Kudos
Reply

1,537 Views
Voxan
Contributor III
Hi there,

you may want to check the Linux BSPs available on our website based on the board you are targeting.
Those contains Uboot already...

Hope this helps...

Regards
0 Kudos
Reply