Best free alternative to Codewarrior for Coldfire?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Best free alternative to Codewarrior for Coldfire?

4,099件の閲覧回数
vier_kuifjes
Senior Contributor I

I'm currently using Codewarrior Special Edition (v7.1a) to compile my CF Lite based projects.

The thing is... my project is constantly flirting with the 128kBytes code size limit of the Special Edition compiler. My next project which I'm about to start may even exceed that limit as it will contain a number of constant arrays.

I can't afford to buy a Codewarrior license. My projects are just a hobby and for personal use only. So a good, less limited alternative may become necessary.

Can anyone help me out?

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,925件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I think codeSourcery could be a good choice, you can get the lite edition here.

This post could be also interesting.

 

 

Emmanuel

0 件の賞賛
返信

1,925件の閲覧回数
RichTestardi
Senior Contributor II

Hi Marc,

 

We also use the free CodeSourcery Lite to build on Linux, and it seems very reasonable.  I, of course, prefer CW. :smileyhappy:

 

I'm guessing you've already done this, but I also find I shrink my code size dramatically (we have a 64k limit, for other reasons) by selecting the following CW compilation options:

 

*no* A6 Stack Frames

yes Register Coloring

yes Instruction Scheduling

yes Peephole

 

And of course, "Optimize For: Smaller Code Size".

 

The A6 Stack Frames was surprising to me -- I thought it would have a huge impact on debuggability, but it did not.

 

-- Rich

0 件の賞賛
返信

1,925件の閲覧回数
bluehacker
Contributor III

hi,how about CodeSourcery Lite? any limit? if it haven't limit in code size..., I think It will be better choice

 

0 件の賞賛
返信