version 10, change s19 file name?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

version 10, change s19 file name?

ソリューションへジャンプ
4,087件の閲覧回数
irob
Contributor V

I'm liking the new Eclipse IDE, but wow so many options!  I can't seem to find where I can change the S19 file name output after a build.  I see the project properties (right click on the root project folder, click on Properties) dialog with its build options, but nothing specific about output file.

 

I also see the Run Configurations (go to the Run menu, click Run Configurations).  In that tree, under the BDM_PandE_Multilink_CyclonePro branch, in the Main tab, there are options for C/C++ application.  These are by default "Project" and "Standard/Project.abs"

 

I tried changing these both to my new name, but the S19 file that is created remains "Project.s19".  Anyone?

ラベル(1)
タグ(1)
1 解決策
3,571件の閲覧回数
irob
Contributor V

Thanks, BlackNight.  I settled on manually (outside of CW10 / Eclipse) renaming the *.abs, *.args, *.map files.  I also had to update the reference to the old name in the .cproject config file.

 

Works fine now.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,571件の閲覧回数
Nik
Contributor III

Proper way:

properties->C/C++ Build/Built Artifacts

3,571件の閲覧回数
bob_walker
Contributor III
0 件の賞賛
返信
3,571件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

if you are using in your project the Burner to create the S19 file, then have a look at the burner.bbl inside the Project_Settings/Linker_Files/burner.bbl:

there is

OPENFILE "%ABS_FILE%.s19"
format=motorola
busWidth=1
origin=0
len=0x1000000
destination=0
SRECORD=Sx
SENDBYTE 1 "%ABS_FILE%"
CLOSE

So you can change the OPENFILE line to whatever you like.

 

BK

0 件の賞賛
返信
3,572件の閲覧回数
irob
Contributor V

Thanks, BlackNight.  I settled on manually (outside of CW10 / Eclipse) renaming the *.abs, *.args, *.map files.  I also had to update the reference to the old name in the .cproject config file.

 

Works fine now.

0 件の賞賛
返信