request enhancement for __SEG_END_ feature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

request enhancement for __SEG_END_ feature

Jump to solution
1,751 Views
rlw
Contributor I

In the SEGMENTS section of the PRM file, named address ranges are defined for use in the PLACEMENT section. While it makes sense for __SEG_END_  to reflect used range for the sections/segments defined in the PLACEMENT section, it would be more useful if __SEG_END_ reflected the defined range for segments defined in the SEGMENTS section.

 

Example:

 

SEGMENTS

    RAM = READ_WRITE 0xFD000'G TO 0xFFDFF'G;

    STACK = NO_INIT 0x3E00 TO 0x3FF;

    ROM_LOW = READ_ONLY 0x7F4000 to 0x7F6BFF;

    ROM_EOL = NO_INIT 0x7F6C00 TO 0x7F6FFF;

    ROM_CAL = NO_INIT 0x7F7000 TO 0x7F7FFF;

    ROM_MID = READ_ONLY 0x7F8000 TO 0x7FBFFF;

    ROM_HI = READ_ONLY 0x7FC000 TO 0x7FFEFF;

    VECTORS = READ_ONLY 0x7FFF10 to 0x7FFFFF;

END

 

PLACEMENT

    DEFAULT_RAM INTO RAM;

    SSTACK INTO STACK;

    DEFAULT_ROM INTO ROM_LOW, ROM_MID, ROM_HI;

    INTVECT INTO VECTORS;

END

 

It would be useful for the address of __SEG_END_ROM_EOL to be 0x7F7000.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,535 Views
CrasyCat
Specialist III

Hello

 

Please refer to following thread for instruction on how to request enhancement in the tool chain.

 

https://community.freescale.com/thread/77166

 

The way SEG_END is implemented today was useful to a lot of customers. So I would not suggest  to change the way it works, but rather add a new command or functionality to the linker.

 

CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,536 Views
CrasyCat
Specialist III

Hello

 

Please refer to following thread for instruction on how to request enhancement in the tool chain.

 

https://community.freescale.com/thread/77166

 

The way SEG_END is implemented today was useful to a lot of customers. So I would not suggest  to change the way it works, but rather add a new command or functionality to the linker.

 

CrasyCat

0 Kudos
Reply