removing processor expert stationary?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

removing processor expert stationary?

7,277件の閲覧回数
irob
Contributor V
Anyone know how to remove Processor Expert stationary? I started using a bean but then removed it. But now all that stationary is created and in opening the project, CW asks me if it should open up the Processor Expert.

Couldn't find this in Help.
ラベル(1)
タグ(1)
0 件の賞賛
返信
11 返答(返信)

3,725件の閲覧回数
CrasyCat
Specialist III
Hello
  Not sure I understand the problem here.
  Do you mean you want to stop using Processor Expert in your project?
 
  This can be done in the following way:
     - Start IDE
     - Open your project
     - Select "ProcessorExpert" -> "Suspend ProcessorExpert from <projectName>"
  This will disconnect Processor Expert from the project.
 
  I hope this helps.
 
CrasyCat
0 件の賞賛
返信

3,725件の閲覧回数
irob
Contributor V
Not just stop using it, I'd like to remove the Processor Expert stationary. Apparently, it's still present even if it's not used such that CW asks me when I start the project if I want to enable PE.

I have to tell it no each time.
0 件の賞賛
返信

3,725件の閲覧回数
CrasyCat
Specialist III

Sorry I do not understand the question here.

Do you mean you want to prevent CodeWarrior from opening the last project it has opened?

What is exactly the problem can you be more explicit and explain what you are doing and what you are seeing on the screen.

CrasyCat

0 件の賞賛
返信

3,725件の閲覧回数
J2MEJediMaster
Specialist I
What I think you've done is (correct me if I'm wrong):

1) You built a project and had the wizard add Processor Expert (PE).

2) You tried PE and didn't like it.

3) You yanked what you thought were some of the files PE uses, but every time you try to use this project, CodeWarrior nails you with a prompt to start PE. Is this correct?

PE installs its own set of start-up code and files. It's presence is pretty pervasive, as the Codewarrior prompt indicates. I'd suggest you start over with a new project, decline the wizard's offer to add PE to the project, and then move your files into the new project uses Project | Add Files...

---Tom
0 件の賞賛
返信

3,725件の閲覧回数
irob
Contributor V
Darth Jedi,

That's almost exactly right with the exception of when I added the PE. For me, it was actually after creating the project. I added a bean and later changed my mind.

But symptoms are still the same. Yes, CW now prompts me to open the PE bean stuff when I open the project.

Not a huge deal. I can still edit code the old fashioned way and leave the PE stuff off. But it's annoying to an **bleep**-retentive coder like myself to see all those extra files littered all over my project.
0 件の賞賛
返信

3,725件の閲覧回数
CrasyCat
Specialist III
Hello
 
I made some additional tests locally. I think I see what you mean now.
Each time you try to open the project there is a box asking you whether you want to
open ProcessorExpert for the project or not.
 
Even if you check the box "Do not ask for that project again" and hit No, the dialog pops up again
next time.
 
I will report that as a defect.
In the mean time to prevent that from happening, the only solution I found is:
    - Close the project in codeWarrior
    - Open a window explorer
    - Browse for your project directory
    - Delete files with extension .pe, .dsk & .G_C from the directory
    - Remove directory *_Data from the project directory
    - Reopen teh project in eth IDE.
 
That should work.
 
CrasyCat
0 件の賞賛
返信

3,725件の閲覧回数
irob
Contributor V
Nope, that didn't fix it for me. The dialog still pops up. There's also a new couple of folders that I assume PE creates. One is CODE and the other DOC. They are both empty for me, but deleting them didn't help. Any other ideas?
0 件の賞賛
返信

3,725件の閲覧回数
ProcessorExpert
Senior Contributor III
Hello,
could you please write the CPU family and version of Processor Expert that you are using?
best regards
Petr Hradsky
Processor Expert Support Team
UNIS
0 件の賞賛
返信

3,725件の閲覧回数
irob
Contributor V
I'm using MC9S08QG8. ProcessorExpert version 3.73 .5 L2
0 件の賞賛
返信

3,725件の閲覧回数
ProcessorExpert
Senior Contributor III

I'm sorry but I haven't reproduced the problem. I have:

- created a new project with PE
- selected the 'Suspend Processor Expert for ..' menu command
- Closed CodeWarrior, re-opened the project and checked the 'Don't ask again' checkbox in the PE dialog.
and the dialog haven't apperaed anymore after next opening...

I recommend you to create a new project without Processor Expert and insert the sources from your current project there. This should definitely help.

best regards
Petr Hradsky

0 件の賞賛
返信

3,725件の閲覧回数
irob
Contributor V
You're right, if the "don't ask again" is checked it won't. I was just curious at what was causing CW to know that the PE stuff was there, even after all those files were deleted.

No problem, that's a simple fix.
0 件の賞賛
返信