"Loading Programming Algorithm " hangs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"Loading Programming Algorithm " hangs

2,098 次查看
juliancox
Contributor V

I am using CW 11, So8QE16 processor and a Multilink Universal FX. The project builds without any errors. When I try to debug the last two lines in the Console window are: -

INF: ;begin_cs

INF: Loading programming algorithm ...

in the bottom right-hand corner of the CW window the information is< -

Downloading 3184 bytes...(99%)

It will remain like this until I try to cancel. 

pastedImage_2.jpg

If I cancel the first activity the other two disappear, but the only way to cancel the remaining activity is to close CW, shut down windows and reboot.

I tried loading another project and it worked fine.

0 项奖励
回复
3 回复数

1,963 次查看
juliancox
Contributor V

Hi Jennie.

It works fine with a different project in the same workspace. To get around the problem I created a new project in a new workspace. I then did a Copy/Paste of all of the source files and the new project worked fine. I have not tried it on another computer.

0 项奖励
回复

1,963 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Good to know the problem was solved.

Have a nice day,

Jennie

0 项奖励
回复

1,963 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

- How it works if you create a new project under a new workspace?

- How it works if you use this project under a new workspace?

- Does  this problem remain same on another computer?


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复