Hello
_LDEC is a runtime function implemented in the ansi library used to decrement a long (32 bit) variable.
In order to be able to link your application you have to add the appropriate ansi library file to your application.
Please refer to {Install}\lib\hc08c\readme.txt to determine which library file to use. This mainly depends on the options you are using to build the application.
Note that when you are programming in ANSI C you may also need a specific startup code.
I would recommend you to go the following way:
- Create a project indicating you want to use ANSI C and assembly language using the wizard.
- Remove the main.c and main.asm file added by the wizard and replace them by your actual source files.
This should allow you to be up and running quickly.
I hope this helps.
CrasyCat