"Add Watch Expression" in External Memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"Add Watch Expression" in External Memory

ソリューションへジャンプ
2,489件の閲覧回数
Ecap
Contributor I

Hello,

 

i work with "Code Warrior 10.2" and "MQX 3.8" on Kinetis K60 target.

I use 512KB FlexBus external memory starting at 0x60000000.

 

In debug on target i 'm not able to see variables content allocated in external memory.

By "Add Watch expression" debug command i see 0xBABABABA.

 

There is a way to solve the problem??

 

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,811件の閲覧回数
konrada
Contributor IV

Check the memory configuration in your debug target (reachable from the "Connection" in the Debug Configurations dialog). Is there a .mem file? Does it describe your memory layout correctly?

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,812件の閲覧回数
konrada
Contributor IV

Check the memory configuration in your debug target (reachable from the "Connection" in the Debug Configurations dialog). Is there a .mem file? Does it describe your memory layout correctly?

0 件の賞賛
返信
1,811件の閲覧回数
Ecap
Contributor I

Yes there is the link to .mem file.

I have changed it according to my memory and now it works! :smileyhappy:

 

Many Thanks! 

0 件の賞賛
返信