problem with windrvr6.inf !!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem with windrvr6.inf !!

ソリューションへジャンプ
6,806件の閲覧回数
Edward_Kang
Contributor I
When installing the CW12_V4_6.exe, which is the CodeWarrior Development Studio for HCS12X Microcontrollers, the setup cannot be finished because of the following problem.
 
Failed to install the INF file(C:\Windows\inf\windrvr6.inf)
Eroor updating the driver(hwid:*WINDRVR6) with the INF file : cannot find the designated file.
 
 
I use Windows Vista Home Premium and I want to know the solution.
(I already did format and setup again to solve the problem, but ..)


Message Edited by Edward.Kang on 2007-09-04 06:56 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,440件の閲覧回数
CrasyCat
Specialist III
Hello
 
CodeWarrior for HCS12 V4.6 does not support Windows Vista.
The future CodeWarrior for HC(S)12(X) V5.0 will support Windows Vista.
This release is planned for end of this year.
 
You may want to look at the following thread
 
Some people could install CodeWarrior HCS12 on Vista and provide some hints.
Note that Freescale did not validate the tools on Vista and we will not provide support for Vista specific issues when running V4.6.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,441件の閲覧回数
CrasyCat
Specialist III
Hello
 
CodeWarrior for HCS12 V4.6 does not support Windows Vista.
The future CodeWarrior for HC(S)12(X) V5.0 will support Windows Vista.
This release is planned for end of this year.
 
You may want to look at the following thread
 
Some people could install CodeWarrior HCS12 on Vista and provide some hints.
Note that Freescale did not validate the tools on Vista and we will not provide support for Vista specific issues when running V4.6.
 
CrasyCat
0 件の賞賛
返信