problem re-installing cw 10.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

problem re-installing cw 10.1

跳至解决方案
1,161 次查看
stav
Contributor II

I installed cw 10.1 and the patches but I could not get rid of one of the build error messages I had asking to install a CW patch. (Environment is win7 -64 targeting kinetis chips btw).

 

I uninstalled the cw eclipse environent, including the .eclipse user directory.

When I tried to re-install it went through the motions, but when i tried to run it it refused, just saying :"an error has occurred. se the logfile in c:\users\..\.metadata\.log 

 

this file (attached) has a long sob story about things it could not resolve, among other complaints.

 

I tried again, attemting to remove any trace of the previous program to allow a completely clean install, but no luck.

my guess is there must be some junk left in the registry that is causing trouble.

 

Any ideas how to get out of this mess and install the thing again?

 

thanks

标签 (1)
0 项奖励
回复
1 解答
950 次查看
stav
Contributor II

Ok for the benefit of the next guy who has this problem, here is the solution:

on Win 7 if the program cannot write to a protected directory (eg programs\...), it will set up a ghost directory which it

will use instead uder the current user's name in the users directory under ...\virtualstore\etc .

 

It did not help that I had admin rights. This was messing up the re-install, until I erased it manually. The uninstall does not handle it.

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
951 次查看
stav
Contributor II

Ok for the benefit of the next guy who has this problem, here is the solution:

on Win 7 if the program cannot write to a protected directory (eg programs\...), it will set up a ghost directory which it

will use instead uder the current user's name in the users directory under ...\virtualstore\etc .

 

It did not help that I had admin rights. This was messing up the re-install, until I erased it manually. The uninstall does not handle it.

 

 

0 项奖励
回复