problem connecting to the board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem connecting to the board

ソリューションへジャンプ
1,287件の閲覧回数
Yuping
Contributor I

Hi All,

 

I have a TSSEVB from Freescale.

I downloaded CodeWarrior v10 for my x64 system and tried to debug one of the microprocessors on the TSSEVB from my PC.

I tried both the 9S08LG32 microprocessor and the 9S08JM60 COMM microcontroller. Neither of them worked. 

 

When I was setting up the debug configuration, I chose P&E HCS08 Multilink\Cyclone Pro for connection, and chose USB HCS08/HCS12/CFV1 Multilink-USB Port as interface. But when I click refresh, there's no available USB port.

 

I had this problem when I was using CodeWarrior 6.3. The driver for the COMM microcontroller couldn't be installed either.

 

Could anyone help with this?

 

Thanks!

 

Yuping

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
897件の閲覧回数
J2MEJediMaster
Specialist I

There are some issues with CodeWarrior interoperating with USB on a 64-bit Windows 7 system. You might want to look at the last few pages of this forum thread for some work-arounds.

 

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
898件の閲覧回数
J2MEJediMaster
Specialist I

There are some issues with CodeWarrior interoperating with USB on a 64-bit Windows 7 system. You might want to look at the last few pages of this forum thread for some work-arounds.

 

---Tom

0 件の賞賛
返信