is it possible to read a working processor and program a non working (but good)one

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is it possible to read a working processor and program a non working (but good)one

1,450件の閲覧回数
pietrotasson
Contributor I

I have a board with a MC9S08SH16 that has lost the Modbus address and I would like to copy the program from a good same processor to re establish communication.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,378件の閲覧回数
pietrotasson
Contributor I

I am using CodeWarrior Development Studio with a Multilink Universal

0 件の賞賛
返信

1,378件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

You can dump the memory as S19 file and then program that file to the other board, see Recovering the FRDM-K64F Bootloader, or: Cloning the Program of a Microcontroller | MCU on Eclipse 

I hope this helps,

Erich

0 件の賞賛
返信