internal linker error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

internal linker error

ソリューションへジャンプ
1,972件の閲覧回数
李宇涛
Contributor I

mwldeppc: alert: internal linker error: File: 'ELF_linker.c' Line: 10151.

现在编译在链接时出现这个错误,想知道在哪里可以查看这个错误的原因,或者说哪里可以找到ELF_linker.c这个文件?

0 件の賞賛
返信
1 解決策
1,963件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi, 

This is internal linker error exception / crash. "ELF_linker.c" has nothing to do with your project source code.

I'd recommend you to install the latest CodeWarrior version (11.x) which contains the latest version of build tools (4.3 build 317) so there is a high chance the linker bug has been already fixed.

Hope it helps.

Stan

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,964件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi, 

This is internal linker error exception / crash. "ELF_linker.c" has nothing to do with your project source code.

I'd recommend you to install the latest CodeWarrior version (11.x) which contains the latest version of build tools (4.3 build 317) so there is a high chance the linker bug has been already fixed.

Hope it helps.

Stan

0 件の賞賛
返信