install codewarrior for linux (eclipse ide)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

install codewarrior for linux (eclipse ide)

2,833 Views
Assaf
Contributor I

hi all.

i managed to install CW using the wizard installation.

while i try to open it - nothing happens.

 

im using ubuntu 14.04 LTS.

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

2,235 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Biton.

the latest CW10.6 doesn't support Linux.

if you work with Kinetis, I suggest you KDS3.0, which can support Linux® 64-bit (Ubuntu 10.04 (deb), RedHat/Centos 7 (rpm))

Kinetis Design Studio Integrated Development |Freescale

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,235 Views
Assaf
Contributor I

Thank you for your help, I tried install version 10.2, as I said - installation ran successfuly but trying to open the application is get no response.

I've needed that cause I've upgraded to windows 10. Finally I it managed to install the 10.6 version on windows.

0 Kudos
Reply