how to use codewarior for a specific demonstration board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use codewarior for a specific demonstration board

2,828件の閲覧回数
aseembansal
Contributor I

I have TWR-S08DC-PT60 demonstration board for MC9S08P family. How do I use codewarrior for this particular family? I found the quick start guide and installed the software but the process explained is not working. When I debug the IDE stops working. What can I do?

 

EDIT1:-

Added images of the errors that keep on appearing on the screen.

I think that it is some error related to the USB cable that I am using. Am I correct?

 

What USB needs to be used with this board?

 

2660_2660.PNGCapture.PNG

2661_2661.PNGCapture1.PNG

 

Message was edited by: Aseem Bansal

ラベル(1)
タグ(1)
0 件の賞賛
返信
6 返答(返信)

2,277件の閲覧回数
aseembansal
Contributor I

I uninstalled the Code warrior development studio, P&E device drivers and PE Micro OSBDM/OSJTAG virtual serial toolkit and then reinstalled code warrior studio as explained in the quick start guide.

It gave the error at the first time but the second time it worked. I don't know how but it worked for once.

That obviously is not a solution but I will keep you guys updated about what I am doing with this problem.

Any suggestions or remedies are most welcome

Thanks in advance

0 件の賞賛
返信

2,278件の閲覧回数
aseembansal
Contributor I

bump

Added more information regarding the problem. Someone please tell if more info is needed to find the solution.

0 件の賞賛
返信

2,278件の閲覧回数
tom_thompson
Contributor III

This looks like a driver or firmware problem. First, make sure you have all of the service packs installed for CodeWarrior. Choose Help > Look for Software Updates and install those. Next, make sure you have the latest drivers from P&E Microsystems installed. They can be downloaded from www.pemicro.com Finally, use this forum thread that has a description of how to force windows to do a driver update.

---Tom

0 件の賞賛
返信

2,278件の閲覧回数
aseembansal
Contributor I

I tried the forum thread

https://community.freescale.com/message/118504#118504

that you asked. I tried to use it but still the same problem is present. Any suggestions about what to do?

Thanks in advance

0 件の賞賛
返信

2,278件の閲覧回数
eckhard
Contributor V

Hello,

I had the same problem with my TWR-S08DC-PT60. I couldn´t use the debugger after the first flashing. I reprogrammed the PT60 with an USB-Multilink and after that the OSBDM worked.  .

My PT60 board has the OSBDM Firmware Build 90 Revision 9. That seems a litte strange. I have a TWR-S08UNIV, wihich has Firmware Build 30 and Revision 21, this is the latest Download from P&E. This board has problems with OSBDM too.

You can enable console logging for the debugger to see what is going wrong. When I try to debug my S08UNIV, sometimes  the initial connetion goes wrong and sometimes after flashing the device the connection after the reset cant be established.

Eckhard

0 件の賞賛
返信

2,278件の閲覧回数
aseembansal
Contributor I

How to enable the console logging?

0 件の賞賛
返信