how to implement a struct in Codewarrior?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to implement a struct in Codewarrior?

1,574 次查看
jessemayfield
Contributor I

I cannot figure out how to implement a structure in Codewarrior?  Any help is greatly appreciated

标签 (1)
0 项奖励
回复
2 回复数

1,431 次查看
trytohelp
NXP Employee
NXP Employee

Hi Jesse,

Probably the answer is more target dependent.

To avoid confusion I recommended you to refer to the right compiler manual.

All documentations are located in the installation folder \CW_MCU_v10.6\MCU\Help\PDF

A compiler manual is available for each architecture.

Inside the manual you will find information and most is the time an example is included too.

If you're using a classic version the same folder \Help\PDF is installed by default too.

Hope this will help.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,431 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jesse,

Which version of Codewarrior ?

And could you say in detail about "implement a structure" , thank !

BR

Alice

0 项奖励
回复