hex file generated by importing *.mcp file in 10.2 code warrior doesnot match with hex file in 6.0 code warrior why?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hex file generated by importing *.mcp file in 10.2 code warrior doesnot match with hex file in 6.0 code warrior why?

1,016 次查看
santoshalagawad
Contributor I

!

标签 (1)
0 项奖励
回复
1 回复

805 次查看
Rick_Li
NXP Employee
NXP Employee

hi Santosh Alagawadi,

the difference should be caused by the different version of compiler!

after imported the classic CW project into Eclipsed CW, the project will be built with the latest version build tool chain.

compare with old build tool chain, the new build tool chain had been made some modification due to the bug fix and performance improving.

if the new generated .hex function well, then, you can ignore these differences!

0 项奖励
回复