hex file generated by importing *.mcp file in 10.2 code warrior doesnot match with hex file in 6.0 code warrior why?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hex file generated by importing *.mcp file in 10.2 code warrior doesnot match with hex file in 6.0 code warrior why?

1,041件の閲覧回数
santoshalagawad
Contributor I

!

ラベル(1)
0 件の賞賛
返信
1 返信

830件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

hi Santosh Alagawadi,

the difference should be caused by the different version of compiler!

after imported the classic CW project into Eclipsed CW, the project will be built with the latest version build tool chain.

compare with old build tool chain, the new build tool chain had been made some modification due to the bug fix and performance improving.

if the new generated .hex function well, then, you can ignore these differences!

0 件の賞賛
返信